Channels

These settings control the real-time baseband and LTE functionality. These parameters are controlled in the LTE FDDn Uplink node, by clicking the FRC Wizard button. Refer to the FRC Wizard.

1. FRC Parameter Setup

Test Case Setup

FRC Selection

LTE FDD Configuration Summary Table

This section defines the LTE/LTE-Advanced FDD DPCCH/DPDCH's buttons. The Restore Default Settings button is available in all of the LTE FDDn Uplink's tree nodes.

Restores all of the LTE/LTE-Advanced FDD channel's parameters to their default conditions.

1. FRC Parameter Setup

Test Case Setup

Indicates the current setting of the Test Case Setup. This field is updated by the FRC Wizard. Click the FRC Wizard button to invoke the FRC Wizard. Refer 3GPP TS 36.141 for more detail.

FRC Selection

Indicates the current setting of the FRC Selection. This field is updated by the FRC Wizard. Click the FRC Wizard button to invoke the FRC Wizard. Refer 3GPP TS 36.141 for more detail.