Subframe Status

The software controls PUCCH transmission based on the subframe configuration.

Refer to UCI.

1. General

2. Subframe States

Transmission Cycle

Subframe #n State

LTE FDD Configuration Summary Table

This section defines the LTE/LTE-Advanced FDD DPCCH/DPDCH's buttons. The Restore Default Settings button is available in all of the LTE FDDn Uplink's tree nodes.

Restores all of the LTE/LTE-Advanced FDD channel's parameters to their default conditions.

1. General

Transmission Cycle

Choice: 10 | 20 | 40

Default: 10

Sets the transmission cycle of the configured PUCCH data pattern in units of subframes.

2. Subframe States

Subframe #n State

Choices: On | Off

Double-click or use the drop-down menu to enable or disable the PUCCH State of the subframe. The subframes which the subframe number is exceeded by Transmission Cycle are not used.