To set up a fixed reference
channel (FRC), for an Advanced LTE TDD Uplink carrier, click the Wizard
button
in the Uplink Setup
node for the LTE
standards to open the FRC Wizard.
Double-click or use the drop-down menu to set the system bandwidth and number of resource blocks for the fixed reference channel.
Any combination of System Bandwidth and Reference Channel can be selected on the FRC Wizard window, and an error check is executed after clicking the OK button.
For Reference Channel A1-8, A1-9, A2-4, and A2-5 are an exception, System Bandwidth and Reference Channel combination is limited. (A1-8 and A2-4 for 10 MHz System Bandwidth, A1-9 and A2-5 for 20 MHz System Bandwidth)
If RB Size of the Reference Channel is larger than the System Bandwidth, an error message is displayed and FRC wizard is aborted.
Double-click or use the
drop-down menu to set the
FRC Type.
The software sets the parameters displayed in the lower section of the
window to predetermined values for the FRC Type and Reference Channel
"A" value (An-n) selected.
Choice:
A1-1 | A1-2 | A1-3 | A1-4 | A1-5 | A1-6 | A1-7 (System Bandwidth is other than 10 MHz or 20 MHz, and FRC Type is FRC for reference sensitivity and in-channel selectivity (QPSK, R=1/3))
A1-1 | A1-2 | A1-3 | A1-4 | A1-5 | A1-6 | A1-7 | A1-8 (System Bandwidth is 10 MHz, and FRC Type is FRC for reference sensitivity and in-channel selectivity (QPSK, R=1/3))
A1-1 | A1-2 | A1-3 | A1-4 | A1-5 | A1-6 | A1-7 | A1-9 (System Bandwidth is 20 MHz, and FRC Type is FRC for reference sensitivity and in-channel selectivity (QPSK, R=1/3))
A2-1 | A2-2 | A2-3 (System Bandwidth is other than 10 MHz or 20 MHz, and FRC Type is FRC for dynamic range (16QAM, R=2/3))
A2-1 | A2-2 | A2-3 | A2-4 (System Bandwidth is 10 MHz, and FRC Type is FRC for dynamic range (16QAM, R=2/3))
A2-1 | A2-2 | A2-3 | A2-5 (System Bandwidth is 20 MHz, and FRC Type is FRC for dynamic range (16QAM, R=2/3))
A3-1 | A3-2 | A3-3 | A3-4 | A3-5 | A3-6 | A3-7 (FRC Type is FRC for performance requirements (QPSK, R=1/3))
A4-1 | A4-2 | A4-3 | A4-4 | A4-5 | A4-6 | A4-7 | A4-8 (FRC Type is FRC for performance requirements (16QAM, R=3/4))
A5-1 | A5-2 | A5-3 | A5-4 | A5-5 | A5-6 | A5-7 (FRC Type is FRC for performance requirements (64QAM, R=5/6))
A17-1 | A17-2 | A17-3 | A17-4 | A17-5 | A17-6 (FRC Type is FRC for performance requirements (256QAM, R=5/6))
A7-1 | A7-2 | A7-3 | A7-4 | A7-5 | A7-6 (FRC Type is FRC for UL timing adjustment (Scenario 1))
A8-1 | A8-2 | A8-3 | A8-4 | A8-5 | A8-6 (FRC Type is FRC for UL timing adjustment (Scenario 2))
Default: Ax-1 Note) x is FRC Type number.
Double-click or use the drop-down menu to set the Ax value for the FRC.
The software adjusts corresponding parameter values in the lower section based on your selection.
Any combination of System Bandwidth and Reference Channel can be selected on the FRC Wizard window, and an error check is executed after clicking the OK button.
For Reference Channel A1-8, A1-9, A2-4, and A2-5 are an exception, System Bandwidth and Reference Channel combination is limited. (A1-8 and A2-4 for 10 MHz System Bandwidth, A1-9 and A2-5 for 20 MHz System Bandwidth)
If RB Size of the Reference Channel is larger than the System Bandwidth, an error message is displayed and FRC wizard is aborted
Range: 0 to the number of resource blocks determined by the System Bandwidth selection.
Default: 0
Set the resource block offset for the FRC.
Choice: Off | On
Default: Off
Double-click or use the drop-down menu to turn the sounding reference signal on or off.
Displays the allocated resource blocks for the selected FRC Type and Reference Channel 'A' value.
Displays the DFT-OFDM symbols per subframe.
Displays the modulation type for the selected FRC Type.
Displays the code rate for the selected FRC Type.
Displays the payload size for the selected FRC Type and Reference Channel 'A' value.
Displays the code block CRC size, in bits, for the selected FRC Type and Reference Channel 'A' value.
Displays the code block CRC size, in bits, for the selected FRC Type and Reference Channel 'A' value.
Displays the number of code blocks for the selected FRC Type and Reference Channel 'A' value.
Displays the coded block size for the selected FRC Type and Reference Channel 'A' value.
Displays the number of bits per subframe for the selected FRC Type and Reference Channel 'A' value.
Displays the number of symbols per subframe for the selected FRC Type and Reference Channel 'A' value.
Displays the maximum throughput, in kbps, for the selected FRC Type and Reference Channel 'A' value.