Click tree view to display read-only information about the system hardware. Expanding the node in the tree view reveals the node, which opens a window where you can change various instrument settings, such as frequency and amplitude.
in theIf you are using an inter-band setup, however, expanding the
node reveals nodes. Clicking an node displays exactly the same read-only information as the node. Expanding an node reveals the nodes that access individual instrument settings.For information about using the software to change instrument settings:
see Instrument for ARB capability with most signal generators
see Instrument (E6640A) for ARB capability with the E6640A EXM
see Instrument (MXG/EXG Real-Time Software) for real-time capability
When using a simulated signal generator connection, <Simulated Hardware> appears in the cell and <Simulated MXG/EXG/ESG/PSG Signal Generator> appears in the cell. N/A appears in most of the other cells.
Click the
button to run a test of the I/O interface connection between the instrument and the PC. performs the same tests as the button.The Self-Tests window
appears and displays the results of the tests. Closing the test dialog
window also closes the hardware node and opens the waveform setup node.
If an error occurs, a red X
appears next to the failed test and an error message is displayed in the
status area.
Click the
button to run a test of the I/O interface connection between the instrument and the PC. performs the same tests as the button.The Test I/O Connections window
appears and displays the results of the tests. Closing the test dialog
window also closes the hardware node and opens the waveform setup node.
If an error occurs, a red X
appears next to the failed I/O connection and an error message is displayed
in the status area.
View the name assigned to the system.
View the hardware configuration type.
View connection details (LAN or GPIB).
View the instrument model number.
View the instrument serial number.
View the instrument firmware revision number.
View the options of the connected instrument. These cells are not displayed when using simulated hardware.