The UCI Tx sequence window displays the currently configured UCI transmission sequence. For the same UE, the UCI channel cannot be transmitted in subframes occupied by UL-SCH processes.
Select a UCI channel in the Channel
Setup node, then click the
button in the Transmission
Configuration cell to open the UCI Tx sequence window.You
can set parameters for each UCI transmission from within the UCI Tx sequence
window.
Click the Config Tools button
to access a
drop-down list
that enables you to set parameters for all UCI Tx sequences to the same
value. The configured parameters are displayed in the Tx Map.
Use the Import tab to navigate to and import a saved transmission sequence.
Use the Export tab to save the current transmission sequence to a file.
Click the cell to toggle the state of the UCI Tx sequence on or off.
Choice: 1 | 1a | 1b |2 | 2a | 2b
Default: 1a
Set the UCI format.
The Modulation type is set by the software based on the selected Format. See Modulation.
The choices available for the HARQ-ACK parameter are based on the selected Format. See HARQ-ACK.
Range: 0 to 65535
Default: 0
Enter a value for the Radio Network Temporary Identifier (RNTI). RNTI only applies to format 2/2a/2b. See 3GPP TS 36.211.
The modulation type for the UCI Tx sequence is set according to the active Format as follows:
Format 1 = N/A
Format 1a = BPSK modulation
Format 1b = QPSK modulation
Format 2 = QPSK modulation
Format 2a = QPSK + BPSK modulation
Format 2b = QPSK + QPSK modulation
The software sets the Data Type according to the active Format, as follows:
Format 1 = SR
Format 1a = HARQ-ACK (1 bit)
Format 1b = HARQ-ACK (2 bits)
Format 2 with Extended Cyclic Prefix:
Select one of the following from the drop-down menu CQI | CQI + HARQ-ACK (1 bit) | CQI+ HARQ-ACK (2 bits)
Format 2a = CQI + HARQ-ACK (1 bit)
Format 2b = CQI + HARQ-ACK (2 bits)its)
For Formats 2, 2a, or 2b, double-click in this cell to open a dialog box from which you can select PN9, PN15, or User Defined Bits as the data for the UCI TX sequence.
Range:
1 to 13 bits (Formats 2, 2a, 2b with Normal Cyclic Prefix or Format 2 with Extended Cyclic Prefix and CQI Data Type)
1 to 12 bits (Format 2 with Extended Cyclic Prefix and CQI + HARQ-ACK (1 bit) Data Type)
1 to 11 bits (Format 2 with Extended Cyclic Prefix and CQI + HARQ-ACK (2 bits) Data Type)
Enter a value for Data Size for Formats 2, 2a,or 2b.
Double-click the HARQ-ACK cell for the sequence you want to configure to open the HARQ-ACK Info Selection dialog box. Select the radio button in the dialog box for the desired HARQ-ACK. The choices available for HARQ-ACK are determined by the active Format as follows:
HARQ-ACK parameter is grayed out (not used)
Choice: ACK | NACK
Default: ACK
Choice: ACK-ACK | ACK-NACK | NACK-ACK | NACK-NACK
Range: 0 to Max Resource Element - 1 - 1
Default: 0
Enter a value for the PUCCH n(1) number.
Displays the numbers of the resource blocks occupied by the PUCCH, separated by a comma. If any of the following are changed: PUCCH Format, N_RB(2), N_CS(1), n(1), n(2), Delta Shift or Delta Offset, the resource block numbers are updated accordingly.
Range: –60 to 0 dB
Default: 0 dB
Enter a power level in dB for the demodulation reference signal for the UCI Tx sequence.