To set up a UL Reference
Measurement Channel (RMC), for an Advanced LTE TDD Uplink carrier,
click the Wizard button in the Uplink Setup node for the LTE
or LTE-A
standards to open the UL RMC Wizard. The following RMC Wizard window represents a superset of the LTE and LTE-A parameters, and some parameters are only valid for the Advanced LTE and Advanced LTE-A carriers (e.g. UE Category).
Double-click or use the drop-down menu to set the system bandwidth and number of resource blocks for the fixed reference channel.
Choice: QPSK | 16QAM
Default: QPSK
Double-click or use the drop-down menu to set the modulation for the reference measurement channel.
For more details, refer to 3GPP TS 36.521-1.
Allocated Resource Blocks
Choice: 1 | 2 | 5 | 6 | 8 | 10 | 15 | 18 | 20 | 24 | 25
Default: 25
Double-click or use the drop-down menu to set the allocated resource blocks for the reference measurement channel. Choice parameters depend on System Bandwidth and Modulation.
For more details, refer to 3GPP TS 36.521-1.
Choice: Lower End | Upper End
Default: Lower End
Double-click or use the drop-down menu to set the resource block (RB) position for the reference measurement channel.
Lower End: PUSCH RBs are placed lower frequency end of system bandwidth.
Upper End: PUSCH RBs are placed upper frequency end of system bandwidth.
For more details, refer to 3GPP TS 36.521-1.
Choice: 1 | 2 | 3 | 4 | 5
Default: 5
System Bandwidth = 10MHz (50RB), Modulation = 16QAM and Allocated Resource Blocks = 30 or 36 or 50 case
Choice: 2 | 3 | 4 | 5
System Bandwidth = 15MHz (75RB), Modulation = 16QAM and Allocated Resource Blocks = 75 case
Choice: 2 | 3 | 4 | 5
System Bandwidth = 20MHz (100RB), Modulation = 16QAM and Allocated Resource Blocks = 75 or 100 case
Choice: 2 | 3 | 4 | 5
All other case
Choice: 1 | 2 | 3 | 4 | 5
If UE Category = 5 case, Set Support 64QAM = on. Otherwise set Support 64QAM = off
Double-click or use the drop-down menu to set the UE Category for the reference measurement channel. Choice parameters depend on System Bandwidth, Modulation and Allocation Resource Blocks.
UE Category 5 case, the parameter Support 64QAM is set on. Otherwise off.
For more details, refer to 3GPP TS 36.521-1.
Displays the channel bandwidth of UL reference measurement channel based on above RMC configurations. This is a read only parameter.
For more details, refer to 3GPP TS 36.521-1.
Display the allocated resource blocks of UL reference measurement channel based on above RMC configurations. This is a read only parameter.
For more details, refer to 3GPP TS 36.521-1.
Displays the allocated resource blocks.
Displays the DFT-OFDM symbols per sub-frame of UL reference measurement channel based on above RMC configurations. This is a read only parameter.
For more details, refer to 3GPP TS 36.521-1.
Choice: QPSK | 16QAM
Default: QPSK
Double-click or use the drop-down menu to set the modulation for the reference measurement channel.
For more details, refer to 3GPP TS 36.521-1.
Displays the target coding rate of UL reference measurement channel based on above RMC configurations. This is a read only parameter.
For more details, refer to 3GPP TS 36.521-1.
Displays the payload size of UL reference measurement channel based on above RMC configurations. This is a read only parameter.
For more details, refer to 3GPP TS 36.521-1.
Displays the transport block CRC of UL reference measurement channel based on above RMC configurations. This is a read only parameter.
For more details, refer to 3GPP TS 36.521-1.
Displays the number of code blocks - C.
Displays the number of code blocks per sub-frame of UL reference measurement channel based on above RMC configurations. This is a read only parameter.
For more details, refer to 3GPP TS 36.521-1.
Total Symbols per Subframe
Display the total symbols per sub-frame of UL reference measurement channel based on above RMC configurations. This is a read only parameter.
For more details, refer to 3GPP TS 36.521-1.
Displays the UE category of UL reference measurement channel based on above RMC configurations. This is a read only parameter.
For more details, refer to 3GPP TS 36.521-1.