Click tree view. The graph view is located at the bottom of the Waveform Setup and Carrier nodes, and in the Library Waveform Manager's Library Manager window (i.e. power Spectrum view only). For multiple antenna configurations, a tab for each antenna port is displayed above the graph view. Click the tab of the antenna port for which you want to view a waveform graph. Click the Waveform tab to display the waveform graph.
or in theThe CCDF, Waveform, and Power Envelope graphs are minimized in the initial view of the Carrier node. To view the graphs, click and drag the border above the CCDF, Waveform, and Power Envelope graphs.
Click
or from the main tool bar to generate an I/Q waveform and plot four different waveform graphs (Power, I+Q, I/Q, and Spectrum) of the current waveform configuration. Changes to the waveform configuration do not appear on the graph until you generate the waveform. The status bar at the bottom of the screen shows waveform generation progress.The
plot is shown in the Figure.
Click the down arrow to open a drop-down menu from which you can select different waveform plots. Selections include Power (shown above), I+Q, I|Q, and Spectrum. Click the button to the left of the arrow to select the next plot type in the list without displaying the menu.