When using multiple instruments as shown in the tree view, inaccurate test data may occur if a combination of the GUI and SCPI is used to set or modify the instrument and test parameters. The software will not reflect changes made outside of the GUI even with the use of the Update from Instrument button. For all tests, use only one method to configure the settings, GUI or SCPI.
When configuring multiple instruments with SCPI instead of using the GUI, the commands must be executed for each instrument.
When using multiple instruments as shown in the tree view, after clicking the State On button, all settings for this window gray out and cannot be changed. To change the settings, first click the State Off button.
1. General |
2. Process States |
---|---|
|
|
This button indicates that the current real-time settings have been applied to the instrument—no action is required. This button is not available when the Apply Needed button is active. When using multiple instruments as shown in the tree view, this button is not displayed. |
|
This button displays in place of the Settings Current button. It indicates that the instrument settings are not currrent and need to be updated with the new software settings. Click this button to update the insturment's settings. This button shows in all windows regardless of where the change was made. When using multiple instruments as shown in the tree view, this button is not displayed. |
Choice: All Processes On | Customize
Default: All Processes On
Double-click or use the drop-down menu to select the process transmission control method.
All Processes On |
Each state of Process [n] is on. |
Customize |
Each state of Process [n] can be configured on or off. |
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:TCONtrol:STATe 1|0|ON|OFF
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:TCONtrol:STATe?
When the state is set to 0 (or OFF), all processes are set to On. When the state is set to 1 (or ON), each state of Process[n] can be configured on or off. The 1 (or ON) of SCPI state command is mapped to Customize on the GUI, 0 (or OFF) is mapped to the All Processes On on the GUI.
Displays the number of HARQ process calculated by the Uplink Downlink Configuration.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:NPRocess?
Choice: On | Off
Default: On
Double-click or use the drop-down menu to select each Process State on or off when the Process Transmission Control is set to Customize.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:TCONtrol:PROCess0|1|2|3|4|5|6:STATe 1|0|ON|OFF
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:TCONtrol:PROCess0|1|2|3|4|5|6:STATe?