The UL-SCH TX window displays the transmission sequence defined in the Channel Setup node for the selected UL-SCH channel.
Select a UL-SCH channel in the Channel
Setup node, then click the
button in the Transmission
Configuration cell to open the UL-SCH Tx sequence
window.
Click the button to access a drop-down list that enables you to set parameters for all transmissions to the same value. The settings configured in the Channel Setup node and the UL-SCH Tx sequence window are displayed in the Tx Map.
Use the Import tab to navigate to and import a saved transmission sequence.
Use the Export tab to save the current transmission sequence to a file.
Refer to the parameter descriptions below and to 3GPP TS 36.211 for additional information.
UL-SCH Tx sequence window (left segment)
UL-SCH Tx sequence window (center segment)
UL-SCH Tx sequence window (right segment)
UL-SCH Tx sequence window (additions to left segment)
UL-SCH Tx sequence window (additions to center segment)
|
Grid Parameters |
Additional MIMO Grid Parameters | ||
|---|---|---|---|
Displays the sequence number.
Displays the radio frame number.
Displays the subframe number (0 to 9) in radio frame.
Choice: On | Off
Default: On
Click to turn on or off the transmission state in the current subframe.
Range:
Type 0 | Type 1
Type 0 (DCI Format 0 and Hopping Mode is not off case)
Default: Type 0
Double-click or use the drop-down menu to select the uplink resource allocation type. In the case DCI Format 0 and Hopping Mode is not off, Type 0 is only available with read only.
Type 0: A set of contiguously allocated virtual resource block which indicated by a starting resource block (Virtual Resource Block Offset) and length (Virtual Resource Block Size).
Type 1: Two sets of resource blocks with each set including one or more consecutive resource block groups of size P same as downlink RBG size for uplink system bandwidth.
See 3GPP TS 36.213 for more information.
Range: 0 to maximum RB size – 1
Default: 0
Enter a value of the resource block offset in RA Type 0 (single clustered) case.
In RA Type 1 (multi-clustered) case the RB Offset is shown for cluster #1 (RBG Start #1/RBG End #1) and cluster #2 (RBG Start #2/RBG End #2) respectively as read-only.
For example, RB Offset is (0, 27) means cluster #1 is 0 RB Offset and cluster #2 is 27 RB Offset.
See 3GPP TS 36.211 and 36.213 for more information.
Range: 1 to maximum RB size
Enter a value of the resource block size in RA Type 0 (single clustered) case.
In RA Type 1 (multi-clustered) case the RB Size is shown for cluster #1 (RBG Start #1/RBG End #1) and cluster #2 (RBG Start #2/RBG End #2) respectively as read-only.
For example, RB Size is (24, 21) means cluster #1 is 24 RB Size and cluster #2 is 21 RB Size.
See 3GPP TS 36.211 and 36.213 for more information.
Choices: Off | On
Sets the re-transmission process of the transport block 1 (codeword 0) for the corresponding PUSCH transmission. (Toggle the new data indicator state or not.)
On: Re-transmission data with next RV index is transmitted. (The new data indicator is not toggled.)
Off: New data is transmitted. (The new data indicator is toggled.)
First transmission of each process is not available to set re-transmission.
For example, when the Number of HARQ Processes is 1 (Assigned Process is 0) and every subframe transmission is on, the re-transmission is not available to the first transmission.
Example: If the eNB receives incorrect data in uplink process #0, it sends a sends a retransmission request (NACK) to the UE. The UE then resends the data that was sent in previous process #0, 8 subframes earlier, starting with the next cycle of process #0. This is done by incrementing the RV Index(1) in the specified sequence (i.e. 0, 2, 3, 1...), up to the maximum number of the retransmission (i.e. a longer Waveform Generation Length, enables a greater number of potential retransmissions). Each complete retransmission can only happen after eight subframes.
Refer to the 3GPP standards, TS36.213 clause 8 and TS36.321 clause 5.4.2 on HARQ operation.
Range: 0 to 31 | Off
Default: 0
Enter the MCS index of the transport block 1 (codeword 0) for the corresponding PUSCH transmission.
When the “Transmission Setting Mode” in UL-SCH is MCS and this parameter is 0 to 28, the “Modulation(1)” and “TBS Index(1)” are automatically selected.
When the “Transmission Setting Mode” in UL-SCH is MCS and this parameter is 29 to 31, manual selection is available for the “Modulation(1)” and “TBS Index(1)”.
When the “Transmission Setting Mode” in UL-SCH is Manual, this is hidden.
When an MCS Index value is selected, the software generates the values for Modulation, TBS Index, and the TB Size according to the 3GPP standards. You can choose to manually enter the TB Size and the modulation, by turning off the MCS Index and the TBS Index parameters. This is required where the control information is transmitted without any data (payload)
See 3GPP TS 36.211, 36.212 and 36.213, for more information.
Choice: QPSK | 16QAM | 64QAM
Default: QPSK
Displays the modulation type of the transport block 1 (codeword 0) for the corresponding PUSCH transmission, when the “Transmission Setting Mode” in UL-SCH is MCS and “MCS Index(1)” is 0 to 28.
In this case this modulation type is automatically selected by the “MCS Index(1)”.
Otherwise use the drop-down menu to select the modulation type of the transport block 1 (codeword 0) for the corresponding PUSCH transmission.
See 3GPP TS 36.211, 36.212 and 36.213, for more information.
Range: 0 to 26
When the “Transmission Setting Mode” in UL-SCH is MCS and “MCS Index(1)” is 0 to 28, this parameter displays the TBS index of the transport block 1 (codeword 0) for the corresponding PUSCH transmission.
In this case this TBS index is automatically selected by “MCS Index(1)”.
When the “Transmission Setting Mode” in UL-SCH is MCS and the “MCS Index(1)” is 29 to 31, you can enter the TBS index of the transport block 1 (codeword 0) for the corresponding PUSCH transmission.
When the “Transmission Setting Mode” in UL-SCH is Manual, it is hidden.
Both TBS index and resource block size determine the transport block size.
See 3GPP TS 36.211, 36.212 and 36.213, for more information.
Range: 0 to 149776
When the “Transmission Setting Mode” in UL-SCH is MCS and “MCS Index(1)” is 0 to 28, this parameter displays the transport block size of the transport block 1 (codeword 0) for the corresponding PUSCH transmission.
In this case this transport block size is automatically selected by “RB Size” and “TBS Index(1)”.
When the “Transmission Setting Mode” in UL-SCH is MCS and the “MCS Index(1)” is 29 to 31, you cam enter the transport block size of the transport block 1 (codeword 0) for the corresponding PUSCH transmission.
When the “Transmission Setting Mode” in UL-SCH is Manual, it is hidden.
See 3GPP TS 36.212 and 36.213, for more information.
Range: 0 to 3
Default: 0
Enter the redundancy version index (RV Index) of the transport block 1 (codeword 0) for the corresponding PUSCH transmission.
If the “RV Index Configuration” parameter is “Auto”, the RV Index is automatically selected by the “RV Index Sequence” and “Retrans(1)” parameter. Otherwise manual selection is available.
See 3GPP TS 36.212 and 36.213, for more information.
Range: –60 to 20 dB
Default: 0 dB
Enter a power level in dB for the demodulation reference signal (DMRS) relative to the carrier power.
Range: 0 to 7
Default: 0
Enter the cyclic shift field index for the corresponding PUSCH transmission.
Cyclic shift for DMRS and orthogonal sequence is given by CS Field Index and layer number.
See 3GPP TS 36.212 and 36.213, for more information.
Choice: On | Off
Default: Off
Click the check box to enable HARQ-ACK in the current subframe.
Choice: Bundling | Multiplexing
Default: Multiplexing
Click the drop down menu to enable the HARQ-ACK Feedback mode in the current subframe.
Range: 0 to 3
Enter a value for the Nbundled sequence index in the current subframe.
Choice: ACK | NACK | ACK-ACK | ACK-NACK | NACK-ACK | NACK-NACK | User Defined Bits
Default: ACK
Click in the cell to open the HARQ-ACK Info Selection dialog box and select the HARQ-ACK information type.
Range:
1 for HARQ-ACK Info = ACK or NACK
2 for HARQ-ACK Info = ACK-ACK, ACK-NACK, NACK-ACK, NACK-NACK
3 to 11 for HARQ-ACK Info = User Defined Bits
12 to 20 for HARQ-ACK Info = User Defined Bits
If User Defined Bits is selected as the HARQ-ACK Info type, enter a value between 3 and 20 for HARQ-ACK Info Size. The software sets the HARQ-ACK Info Size for the other HARQ-ACK Info type selections as shown above.
Refer to 3GPP TS 36.212 and 36.213.
Range: 0 to 14
Default: 0
Enter a value for HARQ-ACK Offset index for the selected transmission.
Choice: On | Off
Default: Off
Select the check box to enable RI multiplexing to the UL-SCH in a specific subframe.
Choice: 0 | 1 | 0-0 | 0-1 | 1-1 | User Defined Bits
Default: 0
Click in the cell to open the RI Info Selection dialog box. Select one of the choices to set the RI Info type.
Refer to 3GPP TS 36.212 and 36.213.
Range:
1 for RI Info = 0 or 1
2 for RI Info = 0-0, 0-1, 1-0 or 1-1
3 to 11 for RI Info = User Defined Bits
12 to 15 for RI Info = User Defined Bits
The software sets the RI Info Size for the other type selections as shown above.
Based on data size (1 bit, 2 bits, 3-11 bits and 12 to 15 bits), the corresponding channel coding of RI Information is used.
Refer to 3GPP TS 36.212 and 36.213.
Range: 0 to 15
Default: 0
Enter a value for RI Offset index in the selected transmission.
Choice: On | Off
Default: Off
Click the check box to enable CQI/PMI multiplexing to the UL-SCH in a specific subframe.
Choice: PN9 | PN15 | User Defined Bits
Default: PN9
Click in the cell to open the CQI/PMI Info Selection dialog box. Select one of the choices to set the CQI/PMI Info type.
Range: 1 to 144
Default: 4
Enter a value for CQI/PMI Info Size.
Refer to 3GPP TS 36.212 and 36.213.
Range: 0 to 15
Default: 0
Enter a value for CQI/PMI Offset index in the selected transmission.
Range:
1 to 4 (1.4MHz)
1 to 6 (3MHz)
1 to 11 (5MHz)
1 to 15 (10MHz)
1 to 17 (15MHz)
1 to 23 (20MHz)
Default: 1
In case of DCI Format 4, enter a value of the Starting RBG Index of Cluster #1 (0). Otherwise it’s hidden.
In case of Resource Allocation Type = Type 1, this parameter is active. Otherwise inactive.
There is an input limitation which is s0 < s1 < s2 < s3.
Note that the resource block index is shown in parentheses.
See 3GPP TS 36.213 for more information.
Range:
1 to 4 (1.4MHz)
1 to 6 (3MHz)
1 to 11 (5MHz)
1 to 15 (10MHz)
1 to 17 (15MHz)
1 to 23 (20MHz)
Default:
2 (1.4MHz)
3 (3MHz)
6 (5MHz)
8 (10MHz)
8 (15MHz)
12 (20MHz)
In case of DCI Format 4, enter a value of the Starting RBG Index of Cluster #1 (s1-1). Otherwise it’s hidden.
In case of Resource Allocation Type = Type 1, this parameter is active. Otherwise inactive.
There is an input limitation which is s0 < s1 < s2 < s3.
Note that the resource block index is shown in parentheses.
See 3GPP TS 36.213 for more information.
Range:
3 to 6 (1.4MHz)
3 to 8 (3MHz)
3 to 13 (5MHz)
3 to 17 (10MHz)
3 to 19 (15MHz)
3 to 25 (20MHz)
Default:
5 (1.4MHz)
5 (3MHz)
8 (5MHz)
10 (10MHz)
10 (15MHz)
14 (20MHz)
In case of DCI Format 4, enter a value of the Starting RBG Index of Cluster #2 (s2). Otherwise it’s hidden.
In case of Resource Allocation Type = Type 1, this parameter is active. Otherwise inactive.
There is an input limitation which is s0 < s1 < s2 < s3.
Note that the resource block index is shown in parentheses.
See 3GPP TS 36.213 for more information.
Range:
3 to 6 (1.4MHz)
3 to 8 (3MHz)
3 to 13 (5MHz)
3 to 17 (10MHz)
3 to 19 (15MHz)
3 to 25 (20MHz)
Default:
6 (1.4MHz)
7 (3MHz)
12 (5MHz)
16 (10MHz)
18 (15MHz)
24 (20MHz)
In case of DCI Format 4, enter a value of the Starting RBG Index of Cluster #1 (s1-1). Otherwise it’s hidden.
In case of Resource Allocation Type = Type 1, this parameter is active. Otherwise inactive.
There is an input limitation which is s0 < s1 < s2 < s3.
Note that the resource block index is shown in parentheses.
See 3GPP TS 36.213 for more information.
Choices: Off | On
Sets the re-transmission process of the transport block 2 (codeword 1) for the corresponding PUSCH transmission. (Toggle the new data indicator state or not.)
On: Re-transmission data with next RV index is transmitted. (The new data indicator is not toggled.)
Off: New data is transmitted. (The new data indicator is toggled.)
This parameter only exists, when the “Number of Codewords” in UL-SCH is 2.
First transmission of each process is not available to set re-transmission. For example, when the Number of HARQ Processes is 1 (Assigned Process is 0) and every subframe transmission is on, the re-transmission is not available to the first transmission.
Example: If the eNB receives incorrect data in uplink process #0, it sends a sends a retransmission request (NACK) to the UE. The UE then resends the data that was sent in previous process #0, 8 subframes earlier, starting with the next cycle of process #0. This is done by incrementing the RV Index(2) in the specified sequence (i.e. 0, 2, 3, 1...), up to the maximum number of the retransmission (i.e. a longer Waveform Generation Length, enables a greater number of potential retransmissions). Each complete retransmission can only happen after eight subframes.
Refer to the 3GPP standards, TS36.213 clause 8 and TS36.321 clause 5.4.2 on HARQ operation.
Range: 0 to 31
Enter the MCS index of the transport block 2 (codeword 1) for the corresponding PUSCH transmission.
When the “Transmission Setting Mode” in UL-SCH is MCS and this parameter is 0 to 28, the “Modulation(2)” and “TBS Index(2)” are automatically selected.
When the “Transmission Setting Mode” in UL-SCH is MCS and this parameter is 29 to 31, manual selection is available for the “Modulation(2)” and “TBS Index(2)”.
When the “Transmission Setting Mode” in UL-SCH is Manual, this is hidden.
When an MCS Index value is selected, the software generates the values for Modulation, TBS Index, and the TB Size according to the 3GPP standards. You can choose to manually enter the TB Size and the modulation, by turning off the MCS Index and the TBS Index parameters. This is required where the control information is transmitted without any data (payload)
This parameter only exists, when the “Number of Codewords” in UL-SCH is 2.
Choice: QPSK | 16QAM | 64QAM
Default: QPSK
When the “Transmission Setting Mode” in UL-SCH is MCS and “MCS Index(2)” is 0 to 28, this parameter displays the modulation type of the transport block 2 (codeword 1) for the corresponding PUSCH transmission.
In this case this modulation type is automatically selected by the “MCS Index(2)”.
Otherwise, you can use the drop-down menu to select the modulation type of the transport block 2 (codeword 1) for the corresponding PUSCH transmission.
This parameter only exists, when the “Number of Codewords” in UL-SCH is 2.
If the “MCS Index” parameter is 0 to 28, the modulation type is automatically selected by the “MCS Index”. Otherwise manual selection is available.
See 3GPP TS 36.211, 36.212 and 36.213, for more information.
Range: 0 to 26
Default: 0
When the “Transmission Setting Mode” in UL-SCH is MCS and “MCS Index(2)” is 0 to 28, this parameter displays the TBS index of the transport block 2 (codeword 1) for the corresponding PUSCH transmission.
In this case this TBS index is automatically selected by “MCS Index(2)”.
When the “Transmission Setting Mode” in UL-SCH is MCS and the “MCS Index(2)” is 29 to 31, you can enter the TBS index of the transport block 2 (codeword 1) for the corresponding PUSCH transmission.
When the “Transmission Setting Mode” in UL-SCH is Manual, this is hidden. Both TBS index and resource block size determine the transport block size.
This parameter only exists, when the “Number of Codewords” in UL-SCH is 2.
See 3GPP TS 36.211, 36.212 and 36.213, for more information.
Range: 0 to 149776
When the “Transmission Setting Mode” in UL-SCH is MCS and “MCS Index(2)” is 0 to 28, this parameter displays the transport block size of the transport block 2 (codeword 1) for the corresponding PUSCH transmission.
In this case this transport block size is automatically selected by “RB Size” and “TBS Index(2)”.
When the “Transmission Setting Mode” in UL-SCH is MCS and the “MCS Index(2)” is 29 to 31, you can enter the transport block size of the transport block 2 (codeword 1) for the corresponding PUSCH transmission.
This parameter only exists, when the “Number of Codewords” in UL-SCH is 2.
See 3GPP TS 36.212 and 36.213, for more information.
Choice: 0 | 1 | 2 | 3
Default: 0
Use the drop-down menu to select the redundancy version index (RV Index) of the transport block 2 (codeword 1) for the corresponding PUSCH transmission.
If the “RV Index Configuration” parameter is “Auto”, the RV Index is automatically selected by the “RV Index Sequence” and “Retrans(2)” parameter. Otherwise manual selection is available.
This parameter only exists, when the “Number of Codewords” in UL-SCH is 2.
See 3GPP TS 36.212 and 36.213, for more information.