Real Time

Go to description Go to description Go to description Go to description Go to description Go to description Go to description

Test Model Wizard

Test Model Type

Choice:

Basic LTE: E-TM1.1 | E-TM1.2 | E-TM2 | E-TM3.1 | E-TM3.2 | E-TM3.3 | E-TM1.1 BC3 CS3 | E-TM1.2 BC3 CS3 | E-TM2 BC3 CS3 | E-TM3.1 BC3 CS3 | E-TM3.2 BC3 CS3 | E-TM3.3 BC3 CS3 | None

Basic LTE-A: E-TM1.1 | E-TM1.2 | E-TM2 | E-TM2a | E-TM3.1 | E-TM3.1a | E-TM3.2 | E-TM3.3 | E-TM1.1 BC3 CS3 | E-TM1.2 BC3 CS3 | E-TM2 BC3 CS3 | E-TM3.1 BC3 CS3 | E-TM3.2 BC3 CS3 | E-TM3.3 BC3 CS3 | None

Default: None

Double-click or use the Closeddrop-down menu to set the Test Model type. The software sets the parameters displayed in the lower section of the window to predetermined values for the Test Model type and Reference Channel “A” value selected.

BC3 CS3 test model choices appear only when Minor Enhancement Update (MEU) Option U03 or greater is valid. Refer to Licenses for more information.

System Bandwidth

Choice: 1.4 MHz (6RB) | 3 MHz (15RB) | 5 MHz (25RB)) | 10 MHz (50RB) | 15 MHz (75RB) | 20 MHz (100RB)

Default:

LTE: 5 MHz (25RB)

LTE-A: 10 MHz (50RB)

Double-click or use the drop-down menu to set the system bandwidth and number of resource blocks (RB). When you select a system bandwidth, the software automatically adjusts the values in the Total Number of Resource Blocks and Total Number of Occupied Sub-carriers cells.

Advanced LTE and LTE-A carriers only: When the system bandwidth is decreased, the DL-SCH Tx Sequence window's RB size, and some of the other data channel's settings, are reconfigured, similar to when a predefined configuration is executed. But, when the system bandwidth is increased, no change to the DL-SCH Tx Sequence window's RB size, or the other data channel's settings occurs.

Auto Carrier Aggregation Configuration

Choice: On | Off

Default On

Click in the cell and use the drop-down arrow to select either On or Off.

 

On

 

Frequency Offset, Cell ID, Uplink Downlink Configuration, Special Subframe Configuration, and Cyclic Prefix are automatically set by the software. In addition for the secondary cells, Uplink Downlink Configuration, Special Subframe Configuration, and Cyclic Prefix become read only and use the same values as the primary cell.

For Cell ID, it is set to the same value as the Component Carrier index number.

 

Off

 

Manually set Frequency Offset, Cell ID, Uplink Downlink Configuration, Special Subframe Configuration and Cyclic Prefix.

Cell ID

Range:   0 to 503

Default:  0 with Auto Carrier Aggregation Configuration set to Off

Same as the CC index number with auto Carrier Aggregation Configuration set to On

With Auto Carrier Aggregation Configuration set to Off, enter a cell ID value.

The software uses this value to set the Physical Layer Cell ID group and sector cells:

Cell ID = (3 x Physical Cell ID group + Physical Cell ID sector).

See 3GPP TS 36.211 for more information.

Waveform Generation Length

Choices: 1 slot (0.5 ms) | 2 slots (1.0 ms) | … | 18 slots (9.0 ms) | 19 slots (9.5 ms) | 1 frame (10 ms) | 2 frames (20 ms) | 3 frames (30 ms) | 4 frames (40 ms)

Default: 1 frame (10 ms)

Double-click or use the drop-down menu to select the waveform generation length.

When the waveform generation length or offset is set, Waveform Generation Length + Waveform Generation Offset <= 1 frame (10 ms) is automatically satisfied by the software.

When the waveform generation length is longer than 1 frame, the waveform generation offset is limited to 0 slot (0.0 ms).

Shorter waveform length choices (< 10 ms) for this parameter are available only when Minor Enhancement Update (MEU) Option U01 or greater is valid. Refer to Licenses for more information.

This parameter appears in the software's GUI only when Minor Enhancement Update (MEU) Option U03 or greater is valid. Refer to Licenses for more information.

Special Subframe Configuration

Range: 0 to 8 (Normal CP), 0 to 6 (Extended CP)

0 to 9 (Normal CP), 0 to 7 (Extended CP)

Default: 0

Coupling: For Basic, Advanced UL, and Advanced DL LTE-A TDD when Auto Carrier Aggregation Configuration is set to On, this setting is read only for the secondary cells that has the same value as the primary cell.

Double-click or use the drop-down menu to select the special subframe configuration. The special subframe configurations are defined in Table 4.2-1 of 3GPP TS 36.211.

0 to 9 (Normal CP) and 0 to 7 (Extended CP) ranges for this parameter are available only for Basic and Advanced LTE-A TDD, and then only for Basic LTE-A TDD when Minor Enhancement Update (MEU) Option U03 or greater is valid. Refer to Licenses for more information.

This parameter appears in the software's GUI only when Minor Enhancement Update (MEU) Option U03 or greater is valid. Refer to Licenses for more information.

Uplink Downlink Configuration

Range: 0 to 6

Default: 0

Coupling: For Basic, Advanced UL, and Advanced DL LTE-A TDD when Auto Carrier Aggregation Configuration is set to On, this setting is read only for the secondary cells that has the same value as the primary cell.

Double-click or use the drop-down menu to select the uplink-downlink configuration.

The supported uplink-downlink configurations are defined in Table 4.2-2 of 3GPP TS 36.211.

In the case of intra-band carrier aggregation, the PCell parameter is editable, but SCell is read-only. With inter-band carrier aggregation, both parameters are editable.

The resource blocks and some parameters are reconfigured by changing the Uplink Downlink Configuration parameter in the same manner as Predefined Configuration.

This parameter appears in the software's GUI only when Minor Enhancement Update (MEU) Option U03 or greater is valid. Refer to Licenses for more information.