The PUSCH transmission is controlled based on the HARQ packet number.
|
1. General |
2. Process States |
|---|---|
|
|
Refer to General Settings
This section defines the LTE/LTE-Advanced TDD DPCCH/DPDCH's buttons. The Restore Default Settings button is available in all of the LTE TDDn Uplink's tree nodes.
|
Restores all of the LTE/LTE-Advanced TDD channel's parameters to their default conditions. |
Choice: All Processes On | Customize
Default: All Processes On
Double-click or use the drop-down menu to select the process transmission control method.
|
All Processes On |
Each state of Process [n] is on. |
|
Customize |
Each state of Process [n] can be configured on or off. |
Displays the number of HARQ process calculated by the Uplink Downlink Configuration.
Choice: On | Off
Default: On
Double-click or use the drop-down menu to select each Process State on or off when the Process Transmission Control is set to Customize.