|
1. UL-SCH Settings |
2. HARQ-ARQ Settings |
3. Hybrid-ARQ ACK/NACK Data Settings |
|---|---|---|
|
|
||
|
|
||
|
|
||
|
|
Refer to HARQ Process Settings.
This section defines the LTE/LTE-Advanced TDD DPCCH/DPDCH's buttons. The Restore Default Settings button is available in all of the LTE TDDn Uplink's tree nodes.
|
Restores all of the LTE/LTE-Advanced TDD channel's parameters to their default conditions. |
Choice: PN9 | PN15 | User Defined
Default: PN9
Double-click or use
the
drop-down menu to select UL-SCH Payload Data Type.
|
PN9 |
Uses PN9 sequence as data bits |
|
PN15 |
Uses PN15 sequence as data bits |
|
User Data |
Uses a user-defined sequence in a file as data bits, represented by binary data. |
Choice: QPSK | 16QAM | 64QAM
Default: QPSK
When Transmission Setting Mode in UL-SCH channel is set to Manual, double-click or use the drop-down menu to select the modulation type for the PUSCH. When the Transmission Setting Mode in the UL-SCH channel is set to Modulation and Coding Scheme (MCS), this value is calculated by the MCS Index. Refer 3GPP TS36.211, Table 8.6.1-1 for more details.
Choice: MCS Index | Manual
Default: MCS
Double-click or use the drop-down menu to select the UL-SCH Payload Configuration Type.
|
MCS Index |
Selects a payload size determined by the Table 7.1.7.2.1-1 ( 3GPP TS36.213) which specifies the permissible combinations of transport block size, resource allocation and modulation scheme that are available for transmission. |
|
Manual |
Allows you to enter any payload size within the minimum (16) and maximum limits (75376) of Table 7.1.7.2.1-1 (3GPP TS36.213). |
Range: 0 to 28
Default: 5
Enter a value of MCS Index. This parameter is used when the Payload Configuration Type is MCS is set to MCS Index.
Displays the value of TBS index. The value is calculated by the MCS Index, Refer to 3GPP TS36.211, Table 8.6.1-1 for more details. This parameter is used when the UL-SCH Payload Configuration Type is set to MCS Index.
Range: 16 to 75376
Default: 2216
When the UL-SCH Payload Configuration Type is set to MCS Index, the payload size is determined by the size of occupied resource blocks and the MCS Index. Refer to 3GPP TS36.213 for more detailed information.
When the UL-SCH Payload Configuration Type is set to Manual, this parameter sets the size of the UL-SCH payload.
Range: 0 to 27
Default: 3
Enter the maximum number of times for the uplink shared channel to be retransmitted.
Default: 0, 2, 3, 1
Entry format: Array of RV Index (Integer 0-3)
Array length: 1 to 28
Enter the RV (redundancy version) Index sequence pattern for verifying HARQ responses. The RV Index data can be entered as a sequence with values of 0, 1, 2, 3 separated by commas. When the specified length of RV index sequence pattern is shorter than the maximum number of retransmission, the pattern is repeated until reaching the maximum length.
Choice: Internal | External
Default: Internal
Double-click or use the drop-down menu to select HARQ ACK/NACK control signal source.
|
Internal |
Uses an internal user-defined signal. |
|
External |
Uses an external signal from AUX ports. |
Choice: All ACK, All NACK, Custom Pattern, User Data
Default: All ACK
Double-click or use the drop-down menu to select the feedback mode for the HARQ ACK/NACK input port. This parameter is used when the Data Source is set to Internal.
|
All ACK |
All ACK sequence |
|
All NACK |
All NACK sequence |
| Custom Pattern | Uses a user-defined sequence as data bits, represented by binary data. |
|
User Data |
Selects a user-defined sequence from an existing file or uses a pattern that you create by entering the character data values: 'A': ACK, 'N': NACK in the Data Source Selection dialog box. |
Choice: Level Triggered | Serial Bits
Default: Level Triggered
Double-click or use the drop-down menu to select the HARQ ACK/NACK control signal source. This parameter is used when the Data Source is set to External.
Default: 0 (Fixed)
Indicates the delay time of the input port for control HARQ ACK/NACK. This parameter is used when HARQ ACK/NACK Data Source is External and the AUX Operating Mode is set to Multiplexed.
Default: 0 (Fixed)
Indicates the delay of HARQ ACK response of the serial data transmission. The unit of the delay number is subframe. This parameter is used when HARQ ACK/NACK Data Source is External and the AUX Operating Mode is set to Dedicated.
Choice: Choice: NACK | ACK
Default: NACK
Double-click or use the drop-down menu to select the default value of HARQ ACK/NACK response of the serial data transmission when the feedback signal is not received. This parameter is used when HARQ ACK/NACK Data Source is External and the AUX Operating Mode is set to Dedicated.