Step 5 - Testing the Equipment Connections

Installation Steps: 1  2  3  4  5  

 

  1. Turn on the instrument and the computer.

  1. Start the Signal Studio software.

  2. Establish communications between the software and the instrument by first selecting New hardware configuration in the Welcome to Agilent Signal Studio for 3GPP W-CDMA dialog box (System Configuration Wizard) that appears.

  3. Select OK and follow the remaining prompts. (Be prepared to enter the instrument's IP/GPIB address.)

Connection

Signal Generator

Key Path

LAN

ESG

PSG

 Utility > GPIB/RS-232 LAN > LAN Setup

GPIB

ESG

PSG

Utility > GPIB/RS-232 LAN > GPIB Address

  1. Signal Studio accepts either the LAN address or hostname. So if you want to use the hostname, just enter the hostname into the software's Hostname/IP Address field. There is no need to access the web interface unless there is a need for the IP address.

If the connection fails or for help with error messages, refer to Troubleshooting.

After making the connection, you can view the instrument's information by selecting Hardware in the tree view

  1. Install the software license:

 

Related Topic

Run Self-test
Test IO Connections