Installation Steps: 1 2 3 4
To generate scenarios using the Option 422 Scenario Generator software, you must have a properly configured PC and a properly configured instrument, as described in the following table.
|
Instruments |
Requirements |
|
E4438C ESG Vector Signal Generator (For more information see the Configuration Guide) |
Firmware revision C.05.74 or later (how to upgrade)
Additional options to consider:
|
|
E8267D PSG Vector Signal Generator (For more information see the Configuration Guide) |
Firmware revision C.05.71 or later (how to upgrade) The following options:
|
|
2 GHz Pentium ® 4 or higher |
|
1.2 GB free disk space at runtime (5 GB or higher recommended) |
|
1024 x 768 screen resolution (1280 x 1024 recommended) |
|
Windows ® Vista Business, Windows ® Vista Ultimate, or Windows ® Vista Enterprise:
|
|
Windows ® XP Professional (service pack 1 or later), Windows® 2000 (service pack 4 or later):
|
|
Installed LAN interface card |
Pentium is a U.S. registered trademark of Intel Corporation.
Windows and MS Windows are U.S. registered trademarks of Microsoft Corporation.
DirectX is a U.S. registered trademark of Microsoft Corporation.
Microsoft is a U.S. registered trademark of Microsoft Corporation.
Adobe, the Adobe Logo, Acrobat and the Acrobat Logo are trademarks of Adobe Systems Incorporated.