When you use the PXI VNAs, you can control the M9168C/E program Step Attenuator module through the VNA firmware. The following commands are available when the launcher includes the M9168C/E.
SENSe:ATTenuatorr:M91Xx | COUNt? | MODule | CHASsis | PATH | SLOT |
Click on a keyword to view the command details.
Applicable Models: PXI VNAs (Read-only) Returns the total number of M9168C/E Attenuator that are connected to the VNA firmware. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. This command is common for all channels and the setting is ignored. |
Examples |
SENS:ATT:M91X:COUN? |
Return Type |
Numeric |
Default |
Not applicable |
Applicable Models: PXI VNAs (Read-Write) Sets and reads the attenuation of the M9168C/E. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
<mod> |
Module number of M9168C/E. The number starts from 1 for the leftmost module of M9168C/E. |
<id> |
Id of the attenuation value, if unspecified, value is set to 1 1: for S parameter sweep 2: for Noise Figure Sweep |
<val> |
Attenuation in dB from 0 to 101dB with 1 dB step. |
Examples |
SENS:ATT:M91X:MOD1:ATT1
10 |
Query Syntax |
SENSe<cnum>:ATTenuator:M91Xx::MODule<mod>:ATTenuation<id>? |
Return Type |
Numeric |
0 |
|
Applicable Models: PXI VNAs (Read Only) Returns the chassis number where the specified M9168C/E module is located. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. This command is common for all channels and the setting is ignored. |
<mod> |
Module number of M9168C/E. The number starts from 1 for the leftmost module of M9168C/E. |
Examples |
SENS:ATT:M91X:MOD1:CHAS? sense2:attenuator:m91xx:module2:chassis? |
Return Type |
Numeric |
Not applicable |
|
Applicable Models: PXI VNAs (Read-Write) Sets and reads the status of M9168C/E control. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
<mod> |
Module number of M9168x. The number starts from 1 for the leftmost module M9168x |
<bool> |
Module control state. Choose from: O or OFF - Skips to control the M9168C/E at the specified channel. 1 or ON - Enables to control the M9168C/E at the specified channel. |
Examples |
SENS:ATT:M91X:MOD1:CONT ON sense2:attenuator:m91xx:module2:control 0 |
Query Syntax |
SENSe<cnum>:ATTenuator:M91Xx:MODule<mod>:CONTrol[:STATe]? |
Return Type |
Boolean |
ON |
|
Applicable Models: PXI VNAs (Read-Write) Sets and reads the path for the M9168C/E. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
<mod> |
Module number of M9168C/E. The number starts from 1 for the leftmost module of M9168C/E. |
<char> |
Path. Choose from: ANY - Fixed attenuator setting NFSource -
NFReceiver - Receiver path during NF measurement
See SENSe:ATT:M91X::MOD:ATT for ID1 and 2 |
Examples |
SENS:ATT:M91X:MOD1:PATH ANY sense2:ATT:M91X:module2:path NFSource |
Query Syntax |
SENSe<cnum>:ATTenuator:M91Xx:MODule<mod>:PATH? |
Return Type |
Char |
ANY |
|
Applicable Models: PXI VNAs (Write Only) Reset the M9168C/E setting at the default value. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. This command is common for all channels and the setting is ignored. |
<mod> |
Module number of M9168C/E. The number starts from 1 for the leftmost module of M9168C/E. |
Examples |
SENS:ATT:M91X:MOD1:RES:IMM sense2:ATT:M91X:module2:reset:immediate |
Return Type |
Not applicable |
Not applicable |
|
Applicable Models: PXI VNAs (Read Only) Reads the slot number where the M9168C/E is located. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. This command is common for all channels and the setting is ignored. |
<mod> |
Module number of M9168C/E. The number starts from 1 for the leftmost module of M9168C/E. |
Examples |
SENS:ATT:M91X:MOD1:SLOT? sense2:ATT:M91X:module2:slot? |
Return Type |
Numeric |
Not applicable |
|