Configures and makes settings for GCA Parallel measurements.
SYSTem:CHANnels:GCSetup: | PARallel | GROup
|
Click on a red keyword to view the command details.
See Also
Learn about: GCA Parallel Measurement
Programming example: Setting Up GCA Parallel Measurement
Applicable Models: M980xA (Read-Write) Sets and reads the GCA Parallel Measurement state. |
|
Parameters |
|
<bool> |
Choose from: ON or 1: GCA parallel measurement are enabled. OFF or 0: GCA parallel measurement are disabled.. |
Examples |
SYST:CHAN:GCS:PAR:ENAB ON system:channels:gcsetup:parallel:enable 0 |
Query Syntax |
SYSTem:CHANnels:GCSetup:PARallel:ENABle? |
OFF |
Applicable Models: M980xA (Read-Write) Sets and reads the group of channels for the GCA Parallel Measurement. |
|
Parameters |
|
<iarray> |
{<number of group>, <start channel No. of group #1>, <end channel No. of group #1>, <start channel No. of group #2>, <end channel No. of group #2>, ... } The first item means number or groups. Next pairs show start/end channel numbers of the group. 1 pair for 1 group. Example: {0} - Couples all existing GCA channels in one group (default setting) {1,1,4} - Couples channel 1-4 in one group {2,1,3,5,7} - Couples channel 1-3 in first group and channels 5-7 in second group |
Examples |
SYST:CHAN:GCS:PAR:GRO 2,1,3,5,7 system:channels:gcsetup:parallel:group 1,1,4 |
Query Syntax |
SYSTem:CHANnels:GCSetup:PARallel:GROup? |
0 |