SYSTem:CONFigure:MWAVe Commands

Controls and queries settings that affect Millimeter Wave measurements.

Click a command to access its description.

SYSTem:CONFigure:MWAVe:CONFigure:ACTive

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:CALibration:DATE

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:CALibration:ENABle

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:CALibration:TIME

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:MODel?

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:OPTion?

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:PORT{1:4}:CALibration:DATE

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:PORT{1:4}:CALibration:ENABle

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:PORT{1:4}:CALibration:TIME

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:PORT{1:4}:MODel?

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:PORT{1:4}:OPTion?

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:PORT{1:4}:SERial?

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:SERial?

SYSTem:CONFigure:MWAVe:CONFigure:ADD

SYSTem:CONFigure:MWAVe:CONFigure:CATalog?

SYSTem:CONFigure:MWAVe:CONFigure:NEW

SYSTem:CONFigure:MWAVe:CONFigure:REMove

SYSTem:CONFigure:MWAVe:FREQuency:LO:MULTiplier

SYSTem:CONFigure:MWAVe:FREQuency:LO:SOURce

SYSTem:CONFigure:MWAVe:FREQuency:LO:STARt?

SYSTem:CONFigure:MWAVe:FREQuency:LO:STOP?

SYSTem:CONFigure:MWAVe:FREQuency:RF:MULTiplier

SYSTem:CONFigure:MWAVe:FREQuency:RF:SOURce

SYSTem:CONFigure:MWAVe:FREQuency:RF:STARt?

SYSTem:CONFigure:MWAVe:FREQuency:RF:STOP?

SYSTem:CONFigure:MWAVe:FREQuency:STARt

SYSTem:CONFigure:MWAVe:FREQuency:STOP

SYSTem:CONFigure:MWAVe:MODule:CATalog?

SYSTem:CONFigure:MWAVe:MODule:FREQuency:STARt

SYSTem:CONFigure:MWAVe:MODule:FREQuency:STOP

SYSTem:CONFigure:MWAVe:MODule:IFGain

SYSTem:CONFigure:MWAVe:MODule:LO:MULTiplier

SYSTem:CONFigure:MWAVe:MODule:LO:STARt?

SYSTem:CONFigure:MWAVe:MODule:LO:STOP?

SYSTem:CONFigure:MWAVe:MODule:POWer:LIMit

SYSTem:CONFigure:MWAVe:MODule:POWer:LO

SYSTem:CONFigure:MWAVe:MODule:REMove

SYSTem:CONFigure:MWAVe:MODule:RF:MULTiplier

SYSTem:CONFigure:MWAVe:MODule:RF:STARt?

SYSTem:CONFigure:MWAVe:MODule:RF:STOP?

SYSTem:CONFigure:MWAVe:PORT{1:4}[:MODule]

SYSTem:CONFigure:MWAVe:PORT{1:4}:FREQuency:STARt

SYSTem:CONFigure:MWAVe:PORT{1:4}:FREQuency:STOP

SYSTem:CONFigure:MWAVe:SERial?

SYSTem:CONFigure:MWAVe:TSET:ALC

SYSTem:CONFigure:MWAVe:TSET:CATalog?

SYSTem:CONFigure:MWAVe:TSET:MIXer

SYSTem:CONFigure:MWAVe:TSET:NAME

SYSTem:CONFigure:MWAVe:TSET:PORT

SYSTem:CONFigure:MWAVe:TSET:PORT:COUNt?

SYSTem:CONFigure:MWAVe:TSET:POWer:LIMit

SYSTem:CONFigure:MWAVe:TSET:POWer:OFFSet

SYSTem:CONFigure:MWAVe:TSET:POWer:SLOPe

SYSTem:CONFigure:MWAVe:TSET:RPANel

See Also

SYSTem:CONFigure:MWAVe:CONFigure:ACTive <string>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set and return the active configuration.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Parameters

 

<string>

The name of the mmWave configuration to activate.

Examples

SYST:CONF:MWAV:CONF:ACT "N5291A Broadband"  'Set to broadband configuration

SYST:CONF:MWAV:CONF:ACT "WR10"  'Set to banded configuration

system:configure:mwave:configure:active "Standard PNA"  'Set to standard PNA configuration

Query Syntax

SYSTem:CONFigure:MWAVe:CONFigure:ACTive?

Return Type

String

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:ACTive:CALibration:DATE?

Applicable Models: N5293A, N5295A, NA5305A, NA5307A

Note: NA520xA PNA-X Pro must use NA5305A/NA5307A frequency extenders.

(Read-only) Return the calibration date of the active configuration's test set. Three integers are returned (year,month,day). All three integers will be 0 if there is no calibration data for the active test set.

Parameters

None

Examples

SYST:CONF:MWAV:CONF:ACT:CAL:DATE?

system:configure:mwave:configure:active:calibration:date?

Return Type

Integer

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:ACTive:CALibration:ENABle <bool>

Applicable Models: N5293A, N5295A, NA5305A, NA5307A

Note: NA520xA PNA-X Pro must use NA5305A/NA5307A frequency extenders.

(Read-Write) Set or get if source linearity cal is enabled.

Parameters

 

<bool>

Choose from:

0 - OFF - Disable source linearity calibration.

1 - ON - Enable source linearity calibration.

Examples

SYST:CONF:MWAV:CONF:ACT:CAL:ENAB ON

system:configure:mwave:configure:active:calibration:enable on

Query Syntax

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:CALibration:ENABle?

Return Type

Boolean

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:ACTive:CALibration:TIME?

Applicable Models: N5293A, N5295A, NA5305A, NA5307A

Note: NA520xA PNA-X Pro must use NA5305A/NA5307A frequency extenders.

(Read-only) Return the calibration time of the active configuration's test set. Three integers are returned (hour,minute,second). All three integers will be 0 if there is no calibration data for the active test set.

Parameters

None

Examples

SYST:CONF:MWAV:CONF:ACT:CAL:TIME?

system:configure:mwave:configure:active:calibration:time?

Return Type

Integer

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:ACTive:MODel?

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-only) Return the model number of the active test set.

Parameters

None

Examples

SYST:CONF:MWAV:CONF:ACT:MOD?

system:configure:mwave:configure:active:model?

Return Type

String

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:ACTive:OPTion?

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-only) Return the option number of the active test set.

Parameters

None

Examples

SYST:CONF:MWAV:CONF:ACT:OPT?

system:configure:mwave:configure:active:option?

Return Type

String

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:ACTive:PORT{1:4}:CALibration:DATE?

Applicable Models: N5293A, N5295A, NA5305A, NA5307A

Note: NA520xA PNA-X Pro must use NA5305A/NA5307A frequency extenders.

(Read-only) Return the calibration date of the active configuration's port. Three integers are returned (year,month,day). All three integers will be 0 if there is no calibration data for the active port.

Parameters

None

Examples

SYST:CONF:MWAV:CONF:ACT:PORT1:CAL:DATE?

system:configure:mwave:configure:active:port1:calibration:date?

Return Type

Integer

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:ACTive:PORT{1:4}:CALibration:ENABle <bool>

Applicable Models: N5293A, N5295A, NA5305A, NA5307A

Note: NA520xA PNA-X Pro must use NA5305A/NA5307A frequency extenders.

(Read-Write) Set or get if source linearity cal is enabled on a specified port.

Parameters

 

<bool>

Choose from:

0 - OFF - Disable source linearity calibration for the specified port.

1 - ON - Enable source linearity calibration for the specified port.

Examples

SYST:CONF:MWAV:CONF:ACT:PORT1:CAL:ENAB ON

system:configure:mwave:configure:active:port1:calibration:enable on

Query Syntax

SYSTem:CONFigure:MWAVe:CONFigure:ACTive:PORTn:CALibration:ENABle?

Return Type

Boolean

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:ACTive:PORT{1:4}:CALibration:TIME?

Applicable Models: N5293A, N5295A, NA5305A, NA5307A

Note: NA520xA PNA-X Pro must use NA5305A/NA5307A frequency extenders.

(Read-only) Return the calibration time of the active configuration's port. Three integers are returned (hour,minute,second). All three integers will be 0 if there is no calibration data for the active port.

Parameters

None

Examples

SYST:CONF:MWAV:CONF:ACT:PORT1:CAL:TIME?

system:configure:mwave:configure:active:port1:calibration:time?

Return Type

Integer

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:ACTive:PORT{1:4}:MODel?

Applicable Models: N5293A, N5295A, NA5305A, NA5307A

Note: NA520xA PNA-X Pro must use NA5305A/NA5307A frequency extenders.

(Read-only) Return the model number of the frequency extender module connected to the specified port number.

Parameters

None

Examples

SYST:CONF:MWAV:CONF:ACT:PORT1:MOD?

system:configure:mwave:configure:active:port1:model?

Return Type

String

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:ACTive:PORT{1:4}:OPTion?

Applicable Models: N5293A, N5295A, NA5305A, NA5307A

Note: NA520xA PNA-X Pro must use NA5305A/NA5307A frequency extenders.

(Read-only) Return the option number of the frequency extender module connected to the specified port number.

Parameters

None

Examples

SYST:CONF:MWAV:CONF:ACT:PORT1:OPT?

system:configure:mwave:configure:active:port1:option?

Return Type

String

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:ACTive:PORT{1:4}:SERial?

Applicable Models: N5293A, N5295A, NA5305A, NA5307A

Note: NA520xA PNA-X Pro must use NA5305A/NA5307A frequency extenders.

(Read-only) Return the serial number of the frequency extender module connected to the specified port number.

Parameters

None

Examples

SYST:CONF:MWAV:CONF:ACT:PORT1:SER?

system:configure:mwave:configure:active:port1:serial?

Return Type

String

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:ACTive:SERial?

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-only) Return the serial number of the test set.

Parameters

None

Examples

SYST:CONF:MWAV:CONF:ACT:SER?

system:configure:mwave:configure:active:serial?

Return Type

String

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:ADD <string>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Add a banded mmWave configuration.

(Read-Write) Add a banded mmWave configuration. Automatically creates a new module and assigns it to all ports.

Note: Deprecated command. Not recommended. Use SYSTem:CONFigure:MWAVe:CONFigure:NEW.

Parameters

 

<string>

The name of the mmWave configuration to add.

Examples

SYST:CONF:MWAV:CONF:ADD "WR10"

system:configure:mwave:configure:add "wr10"

Query Syntax

SYSTem:CONFigure:MWAVe:CONFigure:ADD?

Return Type

String

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:CATalog?

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-only) Returns the list of mmWave configurations.

Parameters

None

Examples

SYST:CONF:MWAV:CONF:CAT?

system:configure:mwave:configure:catalog?

Return Type

Comma-delimited string

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:NEW <string>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Create a configuration with 'No Module' on all ports.

Parameters

 

<string>

The name of the mmWave configuration to add.

Examples

SYST:CONF:MWAV:CONF:NEW "WR10"

system:configure:mwave:configure:new "wr10"

Query Syntax

SYSTem:CONFigure:MWAVe:CONFigure:NEW?

Return Type

String

Default

Not applicable


SYSTem:CONFigure:MWAVe:CONFigure:REMove <string>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Write-only) Remove a mmWave configuration.

Parameters

 

<string>

The name of the mmWave configuration to remove.

Examples

SYST:CONF:MWAV:CONF:REM "WR10"

system:configure:mwave:configure:remove "wr10"

Return Type

Not applicable

Default

Not applicable


SYSTem:CONFigure:MWAVe:FREQuency:LO:MULTiplier <string>,<value>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set the LO multiplier of all modules used in the specified configuration. Read the LO multiplier of the first module in the configuration (by port number). The LO Frequency Range multiplied by this value equals the test port frequency.

(Read-Write) Set and read the LO multiplier value for the specified configuration. The LO Frequency Range multiplied by this value equals the test port frequency. Learn more about frequency settings.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Note: Deprecated command. Not recommended. Use SYSTem:CONFigure:MWAVe:MODule:LO:MULTiplier.

Parameters

 

<string>

The name of the mmWave configuration.

<value>

Choose a value within the range of the analyzer.

Examples

SYST:CONF:MWAV:FREQ:LO:MULT "WR10",8

system:configure:mwave:frequency:lo:multiplier "WR10",8

Query Syntax

SYSTem:CONFigure:MWAVe:FREQuency:LO:MULTiplier? "WR10"

Return Type

Integer

Default

1


SYSTem:CONFigure:MWAVe:FREQuency:LO:SOURce <string>,<source>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set and read the LO source for the specified configuration. Learn more.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Parameters

 

<string>

The name of the mmWave configuration.

<source>

The name of the LO source.

Examples

SYST:CONF:MWAV:FREQ:LO:SOUR "WR10","LO_Source"

system:configure:mwave:frequency:lo:source "WR10","LO_Source"

Query Syntax

SYSTem:CONFigure:MWAVe:FREQuency:LO:SOURce? "WR10"

Return Type

String

Default

Internal LO source


SYSTem:CONFigure:MWAVe:FREQuency:LO:STARt? <string>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-only) Return the calculated LO start frequency of the first module used in the configuration (by port number) using the LO multiplier.

(Read-only) Return the calculated LO start frequency using the LO multiplier for the specified configuration. Learn more about frequency settings.

Note: Deprecated command. Not recommended. Use SYSTem:CONFigure:MWAVe:MODule:LO:STARt?.

Parameters

 

<string>

The name of the mmWave configuration.

Examples

SYST:CONF:MWAV:FREQ:LO:STAR? "WR10"

system:configure:mwave:frequency:lo:start? "WR10"

Return Type

Double

Default

Dependent on the range of the analyzer


SYSTem:CONFigure:MWAVe:FREQuency:LO:STOP? <string>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-only) Return the calculated LO stop frequency of the first module used in the configuration (by port number) using the LO multiplier.

(Read-only) Return the calculated LO stop frequency using the LO multiplierReturn the calculated LO stop frequency of the first module used in the configuration (by port number) using the LO multiplier.for the specified configuration. Learn more about frequency settings.

Note: Deprecated command. Not recommended. Use SYSTem:CONFigure:MWAVe:MODule:LO:STOP?.

Parameters

 

<string>

The name of the mmWave configuration.

Examples

SYST:CONF:MWAV:FREQ:LO:STOP? "WR10"

system:configure:mwave:frequency:lo:stop? "WR10"

Return Type

Double

Default

Dependent on the range of the analyzer


SYSTem:CONFigure:MWAVe:FREQuency:RF:MULTiplier <string>,<value>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set the RF multiplier of all modules used in the specified configuration. Read the RF multiplier of the first module in the configuration (by port number). The RF Frequency Range multiplied by this value equals the test port frequency.

(Read-Write) Set and read the RF multiplier value for the specified configuration. The RF Frequency Range multiplied by this value equals the test port frequency range. Learn more about frequency settings.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Note: Deprecated command. Not recommended. Use SYSTem:CONFigure:MWAVe:MODule:RF:MULTiplier.

Parameters

 

<string>

The name of the mmWave configuration.

<value>

Choose a value within the range of the analyzer.

Examples

SYST:CONF:MWAV:FREQ:RF:MULT "WR10",6

system:configure:mwave:frequency:rf:multiplier "WR10",6

Query Syntax

SYSTem:CONFigure:MWAVe:FREQuency:RF:MULTiplier? "WR10"

Return Type

Integer

Default

1


SYSTem:CONFigure:MWAVe:FREQuency:RF:SOURce <string>,<source>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set and read the RF source for the specified configuration. Learn more.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Parameters

 

<string>

The name of the mmWave configuration.

<source>

The name of the RF source.

Examples

SYST:CONF:MWAV:FREQ:RF:SOUR "WR10","RF_Source"

system:configure:mwave:frequency:rf:source "WR10","RF_Source"

Query Syntax

SYSTem:CONFigure:MWAVe:FREQuency:RF:SOURce? "WR10"

Return Type

String

Default

Internal RF source


SYSTem:CONFigure:MWAVe:FREQuency:RF:STARt? <string>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-only) Return the calculated RF start frequency of the first module used in the configuration (by port number) using the RF multiplier.

(Read-only) Return the calculated RF start frequency using the RF multiplier for the specified configuration. Learn more about frequency settings.

Note: Deprecated command. Not recommended. Use SYSTem:CONFigure:MWAVe:MODule:RF:STARt.

Parameters

 

<string>

The name of the mmWave configuration.

Examples

SYST:CONF:MWAV:FREQ:RF:STAR? "WR10"

system:configure:mwave:frequency:rf:start? "WR10"

Return Type

Double

Default

Dependent on the range of the analyzer


SYSTem:CONFigure:MWAVe:FREQuency:RF:STOP? <string>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-only) Return the calculated RF stop frequency using the RF multiplier for the specified configuration. Learn more about frequency settings.

(Read-only) Return the calculated RF stop frequency of the first module used in the configuration (by port number) using the RF multiplier.

Note: Deprecated command. Not recommended. Use SYSTem:CONFigure:MWAVe:MODule:RF:STOP.

Parameters

 

<string>

The name of the mmWave configuration.

Examples

SYST:CONF:MWAV:FREQ:RF:STOP? "WR10"

system:configure:mwave:frequency:rf:stop? "WR10"

Return Type

Double

Default

Dependent on the range of the analyzer


SYSTem:CONFigure:MWAVe:FREQuency:STARt <string>,<value>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set the start frequency of all modules used in the specified configuration. Read the lowest start frequency of all modules used in the specified configuration.

(Read-Write) Set and read the start frequency for the specified configuration. Learn more about frequency settings.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Note: Deprecated command. Not recommended. Use SYSTem:CONFigure:MWAVe:MODule:FREQuency:STARt.

Parameters

 

<string>

The name of the mmWave configuration.

<value>

The start frequency.

Examples

SYST:CONF:MWAV:FREQ:STAR "WR10",75e9

system:configure:mwave:frequency:start "WR10",75e9

Query Syntax

SYSTem:CONFigure:MWAVe:FREQuency:STAR? "WR10"

Return Type

Double

Default

Dependent on the range of the analyzer


SYSTem:CONFigure:MWAVe:FREQuency:STOP <string>,<value>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set the stop frequency of all modules used in the specified configuration. Read the highest stop frequency of all modules used in the specified configuration.

(Read-Write) Set and read the stop frequency for the specified configuration. Learn more about frequency settings.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Note: Deprecated command. Not recommended. Use SYSTem:CONFigure:MWAVe:MODule:FREQuency:STOP.

Parameters

 

<string>

The name of the mmWave configuration.

<value>

The stop frequency.

Examples

SYST:CONF:MWAV:FREQ:STOP "WR10",75e9

system:configure:mwave:frequency:stop "WR10",110e9

Query Syntax

SYSTem:CONFigure:MWAVe:FREQuency:STOP? "WR10"

Return Type

Double

Default

Dependent on the range of the analyzer


SYSTem:CONFigure:MWAVe:MODule:CATalog?

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Get a list of default and custom modules.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Parameters

None

Examples

SYST:CONF:MWAV:MOD:CAT? "module1,module2,module3"

system:configure:mwave:module:catalog? "module1,module2,module3"

Query Syntax

SYSTem:CONFigure:MWAVe:MODule:CATalog?

Return Type

Comma-delimited string

Default

Not applicable

SYSTem:CONFigure:MWAVe:MODule:FREQuency:STARt <string>,<value>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set or get module start frequency.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed.

Parameters

 

<string>

Module name.

<value>

Start frequency value.

Examples

SYST:CONF:MWAV:MOD:FREQ:STAR "mymodule",75e9

system:configure:mwave:module:frequency:start "mymodule",75e9

Query Syntax

SYSTem:CONFigure:MWAVe:MODule:FREQueny:STARt? <module name>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:MODule:FREQuency:STOP <string>,<value>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set or get module stop frequency.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed.

Parameters

 

<string>

Module name.

<value>

Stop frequency value.

Examples

SYST:CONF:MWAV:MOD:FREQ;STOP "mymodule",110e9

system:configure:mwave:module:frequency:stop "mymodule",110e9

Query Syntax

SYSTem:CONFigure:MWAVe:MODule:FREQueny:STOP? <module name>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:MODule:IFGain <string>,<value>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set or get module IF gain.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed.

Parameters

 

<string>

Module name.

<value>

IF gain.

Examples

SYST:CONF:MWAV:MOD:IFG "mymodule",10

system:configure:mwave:module:ifgain "mymodule",10

Query Syntax

SYSTem:CONFigure:MWAVe:MODule:IFGain? <module name>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:MODule:LO:MULTiplier <string>,<value>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set or get the module LO multiplier.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed.

Parameters

 

<string>

Module name.

<value>

Multiplier.

Examples

SYST:CONF:MWAV:MOD:LO:MULT "mymodule",10

system:configure:mwave:module:lo:multiplier "mymodule",10

Query Syntax

SYSTem:CONFigure:MWAVe:MODule:LO:MULTiplier? <module name>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:MODule:LO:STARt? <string>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Get the calculated LO start frequency.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed.

Parameters

 

<string>

Module name.

Examples

SYST:CONF:MWAV:MOD:LO:STAR? "mymodule"

system:configure:mwave:module:lo:start? "mymodule"

Query Syntax

SYSTem:CONFigure:MWAVe:MODule:LO:STARt? <module name>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:MODule:LO:STOP? <string>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Get the calculated LO stop frequency.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed.

Parameters

 

<string>

Module name.

Examples

SYST:CONF:MWAV:MOD:LO:STOP? "mymodule"

system:configure:mwave:module:lo:stop? "mymodule"

Query Syntax

SYSTem:CONFigure:MWAVe:MODule:LO:STOP? <module name>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:MODule:POWer:LIMit <string>,<value>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set or get module RF Max Power In.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed.

Parameters

 

<string>

Module name

<value>

Power value

Examples

SYST:CONF:MWAV:MOD:POW:LIM "mymodule",10

system:configure:mwave:module:power:limit "mymodule",10

Query Syntax

SYSTem:CONFigure:MWAVe:MODule:POWer:LIMit? <module name>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:MODule:POWer:LO <string>,<value>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set or get the module LO Power In.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed.

Parameters

 

<string>

Module name

<value>

Power value

Examples

SYST:CONF:MWAV:MOD:POW:LO "mymodule",10

system:configure:mwave:module:power:lo "mymodule",10

Query Syntax

SYSTem:CONFigure:MWAVe:MODule:POWer:LO? <module name>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:MODule:REMove <string>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Write-only) Delete a custom module.

Parameters

 

<string>

The module name to remove.

Examples

SYST:CONF:MWAV:MOD:REM "mymodule"

system:configure:mwave:module:remove "mymodule"

Return Type

Not applicable

Default

Not applicable


SYSTem:CONFigure:MWAVe:MODule:RF:MULTiplier <string>,<value>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set or get the module RF multiplier.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed.

Parameters

 

<string>

Module name.

<value>

Multiplier.

Examples

SYST:CONF:MWAV:MOD:RF:MULT "mymodule",10

system:configure:mwave:module:rf:multiplier "mymodule",10

Query Syntax

SYSTem:CONFigure:MWAVe:MODule:RF:MULTiplier? <module name>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:MODule:RF:STARt? <string>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Get the calculated RF start frequency.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed.

Parameters

 

<string>

Module name.

Examples

SYST:CONF:MWAV:MOD:RF:STAR? "mymodule"

system:configure:mwave:module:rf:start? "mymodule"

Query Syntax

SYSTem:CONFigure:MWAVe:MODule:RF:STARt? <module name>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:MODule:RF:STOP? <string>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Get the calculated RF stop frequency.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed.

Parameters

 

<string>

Module name.

Examples

SYST:CONF:MWAV:MOD:RF:STOP? "mymodule"

system:configure:mwave:module:rf:stop? "mymodule"

Query Syntax

SYSTem:CONFigure:MWAVe:MODule:RF:STOP? <module name>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:PORT{1:4}[:MODule] <configuration>,<value>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set or get a module on a specified port.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Parameters

 

<port>

Test set port number.

<configuration>

The name of the mmWave configuration. Use SYSTem:CONFigure:MWAVe:CONFigure:CATalog? for a list of configuration names.

<value>

Module number.

Examples

SYST:CONF:MWAV:PORT1 "WR10",2

system:configure:mwave:port1 "WR10",2

Query Syntax

SYSTem:CONFigure:MWAVe:PORT1? <configuration>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:PORT{1:4}:FREQuency:STARt <configuration>,<value>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set or get the start frequency on a specified port.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Parameters

 

<port>

Test set port number.

<configuration>

The name of the mmWave configuration. Use SYSTem:CONFigure:MWAVe:CONFigure:CATalog? for a list of configuration names.

<value>

The start frequency

Examples

SYST:CONF:MWAV:PORT1:FREQ:STAR  "WR10",75e9

system:configure:mwave:port1:frequency:start "WR10",75e9

Query Syntax

SYSTem:CONFigure:MWAVe:PORT1:FREQuency:STARt? <configuration>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:PORT{1:4}:FREQuency:STOP <configuration>,<value>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set or get the stop frequency on a specified port.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Parameters

 

<port>

Test set port number.

<configuration>

The name of the mmWave configuration. Use SYSTem:CONFigure:MWAVe:CONFigure:CATalog? for a list of configuration names.

<value>

The stop frequency.

Examples

SYST:CONF:MWAV:PORT1:FREQ:STOP "WR10",110e9

system:configure:mwave:port1:frequency:stop "WR10",110e9

Query Syntax

SYSTem:CONFigure:MWAVe:PORT1:FREQuency:STOP? <configuration>

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:MWAVe:SERial?

Applicable Models: N5290A, N5291A

(Read-only) Return the serial number of the mmWave system.

Parameters

None

Examples

SYST:CONF:MWAV:SER?

system:configure:mwave:serial?

"M42147691962"

Return Type

String

Default

Not applicable


SYSTem:CONFigure:MWAVe:TSET:ALC <string>,<bool> OBSOLETED

Note: This command is obsoleted in firmware versions A.20.20.xx and later.

Applicable Models: N5261A, N5262A

(Read-Write) Enable or disable automatic power leveling for the specified configuration. Learn more about test set properties.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Parameters

 

<string>

The name of the mmWave configuration.

<bool>

Choose from:

0 - OFF - Disable automatic power leveling control.

1 - ON - Enable automatic power leveling control.

Examples

SYST:CONF:MWAV:TSET:ALC "WR10",1

system:configure:mwave:tset:alc "WR10",1

Query Syntax

SYSTem:CONFigure:MWAVe:TSET:ALC? "WR10"

Return Type

Boolean

Default

1


SYSTem:CONFigure:MWAVe:TSET:CATalog?

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-only) Returns the list of available test set names.

Parameters

 

Examples

SYST:CONF:MWAV:TSET:CAT?

system:configure:mwave:tset:catalog?

Return Type

Comma-delimited string.

Default

Not applicable


SYSTem:CONFigure:MWAVe:TSET:MIXer <string>,<bool>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Enable or disable mmWave mixer mode to allow mixer testing using the specified configuration. Learn more about test set properties.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Parameters

 

<string>

The name of the mmWave configuration.

<bool>

Choose from:

0 - OFF - Disable mmWave mixer mode.

1 - ON - Enable mmWave mixer mode.

Examples

SYST:CONF:MWAV:TSET:MIXer "WR10",0

system:configure:mwave:tset:mixer "WR10",0

Query Syntax

SYSTem:CONFigure:MWAVe:TSET:MIXer? "WR10"

Return Type

Boolean

Default

0


SYSTem:CONFigure:MWAVe:TSET:NAME <string>,<name>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set and read the test set name for the specified configuration.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Setting the test set name may reset the test set properties to default values, which includes the following:

  • Enabled Modules
  • Mixer Mode
  • IF Gain
  • Route to Rear Panel
  • ALC Enabled
  • Power Limit
  • Power Offset
  • Power Slope

Parameters

 

<string>

The name of the mmWave configuration.

<name>

The name of the test set.

Examples

SYST:CONF:MWAV:TSET:NAME "WR10","N5292A"

system:configure:mwave:tset:name "WR10","N5292A"

Query Syntax

SYSTem:CONFigure:MWAVe:TSET:NAME? "WR10"

Return Type

String

Default

Not applicable


SYSTem:CONFigure:MWAVe:TSET:PORT<port> <configuration>,<val>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) This command is used to enable/disable modules for individual ports on a particular configuration. Disabling a port sets it to No Module. For N5290A/91A and NA53XX Broadband systems, enabling it will detect if a module is physically present and only allows this command on those ports. For custom configurations, enabling will set the port to match the first module used in the configuration (by port number).

(Read-Write) This command enables or disables modules for individual ports on a particular configuration. If an N5292A test set is attached it will detect if a module is physically present and only allow this command on those ports.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Note: Deprecated command. Not recommended. Use SYSTem:CONFigure:MWAVe:PORT:MODule.

Parameters

 

<port>

Test set port number.

<configuration>

The name of the mmWave configuration. Use SYSTem:CONFigure:MWAVe:CONFigure:CATalog? for a list of configuration names.

<val>

Enable/disable test set port. Choose from:

0 - OFF - Disable test set port.

1 - ON - Enable test set port.

Examples

SYST:CONF:MWAV:TSET:PORT1 "WR10",1

system:configure:mwave:tset:port1 "WR10",1

Query Syntax

SYSTem:CONFigure:MWAVe:TSET:PORT1? "N5291A Broadband"

Return Type

Boolean

Default

0


SYSTem:CONFigure:MWAVe:TSET:PORT:COUNt? <string>

Applicable Models: N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-only) Return the number of ports on a test set. Only the test set ports having frequency extenders attached are detected.

Parameters

 

<string>

The name of the mmWave configuration.

Examples

SYST:CONF:MWAV:TSET:PORT:COUNt? "N5291A Broadband"

system:configure:mwave:tset:port:count? "N5291A Broadband"

Return Type

Integer

Default

Not applicable


SYSTem:CONFigure:MWAVe:TSET:POWer:LIMit <string>,<value>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set the maximum RF input power for all modules used in the specified configuration. Read the maximum RF input power of the first module used in the configuration (by port number).

(Read-Write) Set and read the test set power limit for the specified configuration. Learn more about test set properties.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Note: Deprecated command. Not recommended. Use SYSTem:CONFigure:MWAVe:MODule:POWer:LIMit.

Parameters

 

<string>

The name of the mmWave configuration.

<value>

The power limit. Choose a value between -90 and +13 dBm.

Examples

SYST:CONF:MWAV:TSET:POW:LIM "WR10",11

system:configure:mwave:tset:power:limit "WR10",11

Query Syntax

SYSTem:CONFigure:MWAVe:TSET:POWer:LIMit? "WR10"

Return Type

Double

Default

11 dBm


SYSTem:CONFigure:MWAVe:TSET:POWer:OFFSet <string>,<value>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set and read the test set power offset for the specified configuration. Learn more about test set properties.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Parameters

 

<string>

The name of the mmWave configuration.

<value>

The power offset. Choose a value between -30 and +30 dB.

Examples

SYST:CONF:MWAV:TSET:POW:OFFS "WR10",0

system:configure:mwave:tset:power:offset "WR10",0

Query Syntax

SYSTem:CONFigure:MWAVe:TSET:POWer:OFFSet? "WR10"

Return Type

Double

Default

0 dB


SYSTem:CONFigure:MWAVe:TSET:POWer:SLOPe <string>,<value>

Applicable Models: N5252A, N5292A, NA5300A

Note: NA520xA PNA-X Pro must use the NA5300A test set controller.

(Read-Write) Set and read the test set power slope for the specified configuration. Learn more about test set properties.

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Parameters

 

<string>

The name of the mmWave configuration.

<value>

The power slope. Choose a value between -2 dB/GHz and +2 dB/GHz.

Examples

SYST:CONF:MWAV:TSET:POW:SLOP "WR10",.113

system:configure:mwave:tset:power:slope "WR10",.113

Query Syntax

SYSTem:CONFigure:MWAVe:TSET:POWer:SLOpe? "WR10"

Return Type

Double

Default

0.113 dB/GHz


SYSTem:CONFigure:MWAVe:TSET:RPANel <string>,<bool> OBSOLETED

Note: This command is obsoleted in firmware versions A.20.20.xx and later. See also, Route VNA RF to rear panel "SW SRC OUT".

Applicable Models: N5261A, N5262A

(Read-Write) Set and read the status of the RF power routing to the rear panel for the specified configuration:

N5241B/42B/44B/45B/49B: J11 and J8 (4-port only) "SW SRC OUT" connector, or...

N5247B: J6 "RF1 OUT" and J12 "RF2 OUT" (4-port only) connector

Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONFigure:ACTive command is executed.

Parameters

 

<string>

The name of the mmWave configuration.

<bool>

Choose from:

0 - OFF - Disable RF power routing to rear panel.

1 - ON - Enable RF power routing to rear panel "SW SRC OUT" connector (N5241B/42B/44B/45B/49B) or "RF1/2 OUT" connector (N5247B).

Examples

SYST:CONF:MWAV:TSET:RPAN "WR10",1

system:configure:mwave:tset:rpanel "WR10",1

Query Syntax

SYSTem:CONFigure:MWAVe:TSET:RPANel? "WR10"

Return Type

Boolean

Default

1