Receiver Adjustment


This program adjusts the network analyzer receivers for a flat response across its full frequency range. This adjustment is for service only; not for measurement calibration.

NOTE: The is available for M937xA and P937xA only. An adjustment software is provided as an external software for the other products

Required Equipment

See list of supported power meters and sensors.

See VNA Accessories

 

Notes

  • The power sensor depends on the VNA frequency range. Depending on the VNA model, two power sensors may be required to test the full frequency range. The VNA front panel connector type will determine the cable used and if an adapter is required with the power sensor(s).

  • In this adjustment, a power sensor with a specified lower frequency limit of 50 MHz may be used on all instrument that have a lower frequency limit of 10 MHz.  Any added uncertainty is negligible.  

  • If using an older style sensor (without built-in correction factors), refer to your power meter documentation to ensure the proper calibration factors for the power sensor have been entered into a table on the power meter.

  • You must be logged onto the VNA as an Administrator to perform an adjustment. Learn more.

Procedure

  1. Click Utility, then System, then Service, then Adjustment Routines...

  2. At the Adjustments selection, click Receiver Adjustment.

  3. Connect a GPIB cable between the power meter and network analyzer.

  4. Ensure the power sensor(s) are connected to the power meter.

  5. The software presents you with two choices:

    1. Click Inspect Flatness to observe flatness of receiver response versus frequency. Although there is no explicit specification for receiver flatness, Receiver Calibration should improve Transmission and Reflection Tracking error terms which are specified.

    2. Click Calibrate to begin the receiver calibration process. The software prompts you to connect the sensor(s), cable and adapter as needed.

Additional Information

Troubleshooting

In the event there is a problem with Receiver Adjustment, please refer to the "Troubleshooting" chapter in your VNA Service Guide.

Data Storage