Last updated: 2014-11-28
The settings below can be set in active cell operating mode only when the call status is Idle, or in other operating modes.
If BCCH Update Page is set to Auto and you change the settings while your UE is camped to the test set, the test set performs a Broadcast Channel (BCCH) Update Procedure ; If BCCH Update Page is set to Inhibit (the default value) and you change the settings while your UE is camped to the test set, the UE is informed to re-read the BCCH to observe the change (see CALL:BCCHannel:UPDAte:PAGE AUTO).
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the N300, which determines the maximum number of retransmissions of RRC Connection Request message. |
|
Setting |
Range: 0 to 7 |
|
Query |
Range: 0 to 7 |
|
*RST Setting |
0 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:CELL:BCCHannel:N300 0" |
|
Function |
Sets/queries the N312 Link Establishment In-Sync Count , which determines the number of “in-syncs” required when establishing DPCH and the connection status is idle. |
|
Setting |
Range: S1 | S2 | S4 | S10 | S20 | S50 | S100 | S200 | S400 | S600 | S800 | S1000 |
|
Query |
same as setting |
|
*RST Setting |
S1 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:BCCHannel:N312 S1" |
|
Function |
Sets/queries the number of “in-syncs” required when establishing a dedicated channel when in the connection mode. |
|
Setting |
Range: S1 | S2 | S4 | S10 | S20 | S50 | S100 | S200 | S400 | S600 | S800 | S1000 |
|
Query |
same as setting |
|
*RST Setting |
S1 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:BCCHannel:N312:CONNected S1" |
|
Function |
Sets/queries the N313, which determines the maximum number of successive “out of sync” before starts T313. |
|
Setting |
Range: S1 | S2 | S4 | S10 | S20 | S50 | S100 | S200 |
|
Query |
Range: S1 | S2 | S4 | S10 | S20 | S50 | S100 | S200 |
|
*RST Setting |
S2 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:BCCHannel:N313 S2" |
|
Function |
Sets/queries the N315, which specifies the maximum number of successive "in sync" received during T313 is activated. |
|
Setting |
Range: S1 | S2 | S4 | S10 | S20 | S50 | S100 | S200 | S400 | S600 | S800 | S1000 |
|
Query |
Range: S1 | S2 | S4 | S10 | S20 | S50 | S100 | S200 | S400 | S600 | S800 | S1000 |
|
*RST Setting |
S50 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:BCCHannel:N315 S50" |
|
Function |
Sets/queries the T300, which determines how long UE will wait for RRC connection setup after sending RRC Connection Request message. |
|
Setting |
Range: MS400 | MS600 | MS800 | MS1000 | MS1200 | MS1400 | MS1600 | MS1800 | MS2000 | MS3000 | MS4000 | MS6000 | MS8000 |
|
Query |
same as setting |
|
*RST Setting |
MS400 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:CELL:BCCHannel:T300 MS400" |
|
Function |
Sets/queries the T308 timer. |
|
Setting |
Range: MS40 | MS80 | MS160 | MS320 |
|
Query |
same as setting |
|
*RST Setting |
MS40 |
|
Requirements |
Test Application Revision: A.03.00 and above |
|
Programming Example |
"CALL:BCCHannel:T308 MS40" |
|
Function |
Sets/queries the T312, which determines how long UE will wait to get the N312 Link Establishment In-Sync Count (Idle) when establishing DPCH and the connection status is Idle. |
|
Setting |
Range: 1 to 15 |
|
Query |
Range: 1 to 15 |
|
*RST Setting |
1 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:BCCHannel:T312 1" |
|
Function |
Sets/queries the T312, which determines how long UE will wait to get the N312 Link Establishment In-Sync Count (Idle) when establishing DPCH in the connection mode. |
|
Setting |
Range: 1 to 15 |
|
Query |
Range: 1 to 15 |
|
*RST Setting |
1 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:BCCHannel:T312:CONNected 1" |
|
Function |
Sets/queries the T313, which determines how long UE will wait to get N315 “in-syncs” after it detects N313 “out-of-sync”, before it triggers the radio link failure procedure. |
|
Setting |
Range: 0 to 15 |
|
Query |
Range: 0 to 15 |
|
*RST Setting |
3 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:BCCHannel:T313 3" |
|
Function |
Sets/queries the T3212 timer. |
|
Setting |
Range: 0 to 255 decihours |
|
Query |
Same as setting |
|
*RST Setting |
0 |
|
Requirements |
Test Application Revision: A.03.00 and above |
|
Programming Example |
"CALL:BCCHannel:T3212 0" |
|
Function |
Sets/queries the BCCH Update Page state. If it is set to Auto and you change the SIB settings while your UE is camped to the test set, the test set performs a Broadcast Channel (BCCH) Update Procedure (SIB Contents); If it is set to Inhibit (the default value) and you change the SIB settings while your UE is camped to the test set, the UE is informed to re-read the BCCH to observe the change. See Broadcast Channel (BCCH) Update Procedure (SIB Contents). |
|
Setting |
Range: AUTO | INHibit |
|
Query |
Range: AUTO | INH |
|
*RST Setting |
INH |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:BCCHannel:UPDAte:PAGE INH" |