CALL:END

Last updated: 2014-11-28

For more information on the GPIB Command conventions, see GPIB Command conventions

CALL:END[:AUTO]

Function

Disconnects the active service.

The function is used in active cell mode: if call status is Idle, the function is ignored; else if call status is Connected, the function initiates a BS Release procedure; else the function aborts the current call processing operations and returns call status to Idle.

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:END"

CALL:END:AMR

Function

Disconnects any AMR voice calls in progress. Aborts any outstanding registrations or base station pages in progress as well as mobile station originations.

Requirements

Test Application Revision: A.10.00 and above

Programming Example

"CALL:END:AMR"

CALL:END:PSData

Function

Disconnects any PS Data connection that is in progress.

Requirements

Test Application Revision: A.10.00 and above

Programming Example

"CALL:END:PSData"