Last updated: 2010-03-10
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the Primary E-RNTI (in Hex). This setting determines the primary E-RNTI that is used on the E-AGCH. This is the ID that test set will use when it is to transmit data to the UE in Active Cell. |
|
Setting |
Range: 0 to FFFF |
|
Query |
Range: 0 to FFFF |
|
*RST Setting |
AAAA |
|
Requirements |
Test Application Revision: A.05.00 and above |
|
Programming Example |
"CALL:HSUPa:ERNTi 'AAAA'" |
|
Function |
Sets/queries the UE Reported E-DCH Category. |
|
Query |
Range: 1-6, NAN |
|
*RST Setting |
NAN |
|
Requirements |
Test Application Revision: A.05.00 and above |
|
Programming Example |
"CALL:HSUPa:MS:REPorted:EDCHannel:CATegory?" |
|
Function |
Queries the HSUPA Real Time Results in the following order:Exp MAC-e PDU Num, Throughput, ACKs, NACKS |
|
Query |
Range: Exp MAC-e PDU Num: 0 to 200000 Blocks, 9.91E +37 (Null) Throughput: 0 to 99999.999 Kbps, 9.91E +37 (Null) ACKs: 0 to 200000 Blocks, 9.91E +37 (Null) NACKS: 0 to 200000 Blocks, 9.91E +37 (Null) |
|
*RST Setting |
9.91E +37, 9.91E +37, 9.91E +37, 9.91E +37 |
|
Requirements |
Test Application Revision: A.09.00 and above |
|
Programming Example |
"CALL:HSUPa:RTIMe:RESults:ALL?" |
|
Function |
Sets/queries the PS_Data_Channel_Configuration. |
|
Setting |
Range: FIXed | FLEXible |
|
Query |
Range: FIXed | FLEXible |
|
*RST Setting |
FIXed |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:HSUPa:SERVice:PSData:CHANnel:CONFig FIXed" |
|
Function |
Sets/queries the E_PUCH_HS_PDSCH_Timeslot_Config. |
|
Setting |
Range: five character string with value of "U", "D", and "-" "U" denotes the timeslot used for E-PUCH, "D" denotes the timeslot used for HS-PDSCH, and "-" denotes the timeslot is idle. Note that "U" is in the front of "D", and at least one "U" and one "D" are required. |
|
Query |
Range: five character string with value of "U", "D", and "-" |
|
*RST Setting |
UUUD- |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:HSUPa:SERVice:PSData:DATachannel:TSConfig UUUD-" |
|
Function |
Sets/queries the PS_Data_Control_Channel_DL_DPCH_Timeslot_Config. |
|
Setting |
Range: TS0 | TS6 |
|
Query |
Range: TS0 | TS6 |
|
*RST Setting |
TS0 |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:HSUPa:SERVice:PSData:DPCHannel:TSLot TS6" |
|
Function |
Sets/queries the PS_Data_E_PUCH_OVSF. |
|
Setting |
Range: SF1 | SF2 | SF4 | SF8 | SF16 |
|
Query |
Range: SF1 | SF2 | SF4 | SF8 | SF16 |
|
*RST Setting |
SF1 |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:HSUPa:SERVice:PSData:EPUChannel:OVSF SF16" |
|
Function |
Sets/queries the PS_Data_HS_PDSCH_Channel_Codes . |
|
Setting |
Range: 1 to 16 |
|
Query |
Range: 1 to 16 |
|
*RST Setting |
16 |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:HSUPa:SERVice:PSData:HSPDschannel:CCODe:NUMBer 16" |
|
Function |
Sets/queries the PS_Data_HS_PDSCH_OVSF. |
|
Setting |
Range: SF1 | SF16 |
|
Query |
Range: SF1 | SF16 |
|
*RST Setting |
SF1 |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"CALL:HSUPa:SERVice:PSData:HSPDschannel:OVSF SF16" |
|
Function |
Sets/queries the E-DCH FRC Type. This is defined according to 3GPP TS 34.122 Annex C.6.1.2.1 to C.6.2.1.3. This setting can only be changed while the Call Status is IDLE. |
|
Setting |
Range: FRC1a | FRC1b | FRC2 | FRC3 |
|
Query |
Range: FRC1a | FRC1b | FRC2 | FRC3 |
|
*RST Setting |
FRC3 |
|
Requirements |
Test Application Revision: A.05.00 and above |
|
Programming Example |
"CALL:HSUPa:SERVice:RBTest:FRC:TYPE FRC3" |
|
Function |
Sets/queries the E-DCH Max Number of Retransmission. This setting determines the maximum number of retransmissions a HARQ process in the UE that will perform for a given block of data before giving up and moving onto a new block of data. |
|
Setting |
Range: 0 to 15 |
|
Query |
Range: 0 to 15 |
|
*RST Setting |
3 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"CALL:HSUPa:SERVice:RBTest:HARQ:RETRans:MAXimum 3" |
|
Function |
Sets/queries the E-DCH Retransmission Timer. This setting determines the retransmission timer a HARQ process in the UE that will wait for the acknowledgement of a given block of data before giving up and moving onto a new block of data. |
|
Setting |
Range: MS10 | MS15 | MS20 | MS25 | MS30 | MS35 | MS40 | MS45 | MS50 | MS55 | MS60 | MS65 | MS70 | MS75 | MS80 | MS85 | MS90 | MS95 | MS100 | MS110 | MS120 | MS140 | MS160 | MS200 | MS240 | MS280 | MS320 | MS400 | MS480 | MS560 |
|
Query |
Range: MS10 | MS15 | MS20 | MS25 | MS30 | MS35 | MS40 | MS45 | MS50 | MS55 | MS60 | MS65 | MS70 | MS75 | MS80 | MS85 | MS90 | MS95 | MS100 | MS110 | MS120 | MS140 | MS160 | MS200 | MS240 | MS280 | MS320 | MS400 | MS480 | MS560 |
|
*RST Setting |
MS60 |
|
Requirements |
Test Application Revision: A.05.00 and above |
|
Programming Example |
"CALL:HSUPa:SERVice:RBTest:HARQ:RETRans:TIMer MS60" |
|
Function |
Sets/queries the RB Test Mode Uplink E-DCH RLC SDU size. This setting determines the uplink RLC SDU size specified for the E-DCH transport channel in the Close UE Test Loop message sent during a HSUPA RB Test Mode call. The default is chosen to ensure the maximum throughput under FRC2 can be achieved (in this case, the loopback RLC SDU would be just fit into 8 UM RLC PDUs. The E-DCH RLC SDU size to achieve maximum throughput under other FRCs is less than FRC2’s). |
|
Setting |
Range: 72 to 2608 |
|
Query |
Range: 72 to 2608 |
|
*RST Setting |
2608 |
|
Requirements |
Test Application Revision: A.05.00 and above |
|
Programming Example |
"CALL:HSUPa:SERVice:RBTest:RLCSdu:SIZE 2608" |
|
Function |
Sets/queries the E-AGCH Absolute Grant (Power) Value. This parameter controls the next absolute grant that the test set will transmit to the UE on E-AGCH during a HSPA connection. The UE will interpret this value according to the Table 26A in 3GPP 25.222 s4.10.1.1. |
|
Setting |
Range: 0 ~ 31 |
|
Query |
Range: 0 ~ 31 |
|
*RST Setting |
31 |
|
Requirements |
Test Application Revision: A.05.00 and above |
|
Programming Example |
"CALL:HSUPa:SGRant:ABSolute:VALue 31" |