Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
| Function | Generates an AMR voice page attempt to the mobile station. If the call attempt fails, the test set returns to the idle call processing state. | 
| Requirements | Test Application Revision: A.10.00 and above | 
| Programming Example | "CALL:ORIGinate:AMR" | 
| Function | Generates a page attempt to the mobile station. | 
| Requirements | Test Application Revision: A.02.00 and above | 
| Programming Example | "CALL:ORIGinate" | 
| Function | Returns 1 if the page attempt is excuted, or 0 if it is not. | 
| Query | 1|0 | 
| Requirements | Test Application Revision: A.02.00 and above | 
| Programming Example | "CALL:ORIGinate:DONE?" | 
| Function | Returns 1 in the test set's output queue when the page attempt is done, otherwise returns 0. Controlling program hangs on this query until the 1 is retrieved. | 
| Query | 1|0 | 
| Requirements | Test Application Revision: A.02.00 and above | 
| Programming Example | "CALL:ORIGinate:OPComplete?" | 
| Function | Forces an overlapped command to execute in a sequential page attempt. | 
| Requirements | Test Application Revision: A.02.00 and above | 
| Programming Example | "CALL:ORIGinate:SEQuential" | 
| Function | Forces the test set to wait until the page attempt is done before executing any more commands. | 
| Requirements | Test Application Revision: A.02.00 and above | 
| Programming Example | "CALL:ORIGinate:WAIT" |