For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the vocoder calibration type. See Calibration Type. |
|
Setting |
Range: AOPath|AIPath|ICODec |
|
Query |
Range: AOP|AIP|ICOD |
|
*RST Setting |
AOPath |
|
Requirements |
Test Application Revision: A.09.00 and above |
|
Programming Example |
"CALL:RTVocoder:CALibration:TYPE:TDSCdma AOPath" |
|
Function |
Sets/queries the headroom of the decoded data samples to the full scale of the DAC (Digital to Analog Converter). See Real-Time Vocoder Headroom Information. |
|
Setting |
Range: 0.0 to 100 dB, 9.91E+37 (NAN) Resolution: 0.1 dB |
|
Query |
Same as the setting |
|
*RST Setting |
9.91E+37 (NAN) |
|
Requirements |
Test Application Revision: A.09.00 and above |
|
Programming Example |
"CALL:RTVocoder:DECoder:HEADroom:TDSCdma 36" |
|
Function |
Sets/queries the headroom of the audio samples to the full scale of the ADC (Analog to Digital Converter). See Real-Time Vocoder Headroom Information. |
|
Setting |
Range: 0.0 to 100 dB, 9.91E+37 (NAN) Resolution: 0.1 dB |
|
Query |
Same as the setting |
|
*RST Setting |
9.91E+37 (NAN) |
|
Requirements |
Test Application Revision: A.09.00 and above |
|
Programming Example |
"CALL:RTVocoder:ENCoder:HEADroom:TDSCdma 36" |
|
Function |
Sets/queries the peak voltage of the analog audio signal that is applied at the test set's AUDIO IN connector. The units (V|mV) are optional. If no units are specified, then units default to V. See Expected Audio In Peak Voltage. |
|
Setting |
Range: 0.001 to 2.0 V Resolution: 1 mV |
|
Query |
Same as the setting |
|
*RST Setting |
2.0 V |
|
Requirements |
Test Application Revision: A.09.00 and above |
|
Programming Example |
"CALL:RTVocoder:INPut:VOLTage:TDSCdma 1" |
|
Function |
Sets/queries the vocoder operating mode. See Operating Mode. |
|
Setting |
Range: NORMal|CALibration |
|
Query |
Range: NORM|CAL |
|
*RST Setting |
NORMal |
|
Requirements |
Test Application Revision: A.09.00 and above |
|
Programming Example |
"CALL:RTVocoder:OPERating:MODE:TDSCdma CALibration" |
|
Function |
Sets/queries the vocoder Audio Out Frequency, see Audio Out Frequency. |
|
Setting |
Range: 300 Hz to 1100 Hz Resolution: 1.0 Hz |
|
Query |
Same as setting |
|
*RST Setting |
1000Hz |
|
Requirements |
Test Application Revision: A.09.00 and above |
|
Programming Example |
"CALL:RTVocoder:OUTPut:FREQuency:TDSCdma 1000Hz" |
|
Function |
Sets/queries the maximum audio peak output level that is produced on the test set's AUDIO OUT connector according to the voice data received on the R-Traffic/R-FCH channel. The units (V|mV) are optional. If no units are specified, then units default to V. See Maximum Audio Out Peak Voltage. |
|
Setting |
Range: 0.0 to 5.0 V Resolution: 0.1 mV |
|
Query |
Same as setting |
|
*RST Setting |
0.0 V |
|
Requirements |
Test Application Revision: A.09.00 and above |
|
Programming Example |
"CALL:RTVocoder:OUTPut:VOLTage:TDSCdma 350MV" |
|
Function |
Sets/queries whether or not the voice activity detection algorithm is implemented in the speech codec. See Voice Activity Detection State. |
|
Setting |
Range: 1|ON | 0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.09.00 and above |
|
Programming Example |
"CALL:RTVocoder:VADetection:TDSCdma off" |
|
Function |
Sets/queries the voice activity detection algorithm. See Voice Activity Detection Algorithm. |
|
Setting |
Range: OPTion1|OPTion2 |
|
Query |
Range: OPT1|OPT2 |
|
*RST Setting |
OPT1 |
|
Requirements |
Test Application Revision: A.09.00 and above |
|
Programming Example |
"CALL:RTVocoder:VADetection:AMRate:ALGorithm:TDSCdma OPT1" |