Last updated: 2010-05-05
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the authentication algorithm. |
|
Setting |
Range: TEST34108 | MILenage |
|
Query |
Range: TEST34108 | MILenage |
|
*RST Setting |
TEST34108 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SECurity:AUTHenticate:ALGorithm MILenage" |
|
Function |
Sets/queries the AMF value. |
|
Setting |
Range: 0 to FFFF (String of 4 characters from the set 0123456789aAbBcCdDeEfF) |
|
Query |
Range: "0000" to "FFFF" |
|
*RST Setting |
"0000" |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SECurity:AUTHenticate:AMF '0000'" |
|
Function |
Sets/queries the authentication key. |
|
Setting |
Range: 0 to FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF (String of 32 characters from the set 0123456789aAbBcCdDeEfF) |
|
Query |
Range: "00000000:00000000:00000000:00000000" to "FFFFFFFF:FFFFFFFF:FFFFFFFF:FFFFFFFF" (The return string is enclosed by double quotes and is always four colon separated groups in the order of upper, upper middle, lower middle and lower, each group with 8 characters from the set 0123456789ABCDEF) |
|
*RST Setting |
"4147494C:454E5420:54454348:4E4F0000" |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SECurity:AUTHenticate '4147494C454E5420544543484E4F0000'" |
|
Function |
Sets/queries whether the operator variant authentication algorithm contains the OP or Opc. |
|
Setting |
Range: OP|OPC |
|
Query |
Range: OP|OPC |
|
*RST Setting |
OPC |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SECurity:AUTHenticate:OPVariant:PTYPe OPC" |
|
Function |
Sets/queries the value of the operator variant authentication algorithm. |
|
Setting |
Range: 0 to FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF (String of 32 characters from the set 0123456789aAbBcCdDeEfF) |
|
Query |
Range: "00000000:00000000:00000000:00000000" to "FFFFFFFF:FFFFFFFF:FFFFFFFF:FFFFFFFF" |
|
*RST Setting |
"00000000:00000000:00000000:00000000" |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SECurity:AUTHenticate:OPVariant:PVALue '00000000:00000000:00000000:00000000'" |
|
Function |
Sets/queries the random (RAND) value when the current format is TD-SCDMA. |
|
Setting |
Range: 0 to FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF (String of 32 characters from the set 0123456789aAbBcCdDeEfF) |
|
Query |
Range: "00000000:00000000:00000000:00000000" to "FFFFFFFF:FFFFFFFF:FFFFFFFF:FFFFFFFF" (The return string is enclosed by double quotes and is always four colon separated groups in the order of upper, upper middle, lower middle and lower, each group with 8 characters from the set 0123456789ABCDEF) |
|
*RST Setting |
"00000000:00000000:00000000:00000001" |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SECurity:AUTHenticate:RANDom:TDSCdma '00000000:00000000:00000000:00000001'" |
|
Function |
Queries the authentication result in GMM when using TD-SCDMA application:
|
|
Query |
Range: SUCCess| MSFAILMAC | MSFAILSYNC | MSFAILUNKNOWN | RESLENERR | RESNOTMATCH | NULL |
|
*RST Setting |
NULL |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SECurity:AUTHenticate:RESult:GMM:TDSCdma?" |
|
Function |
Queries the authentication result in MM when using TD-SCDMA application:
|
|
Query |
Range: SUCC| MSFAILMAC | MSFAILSYNC | MSFAILUNKNOWN | RESLENERR | RESNOTMATCH | NULL |
|
*RST Setting |
NULL |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SECurity:AUTHenticate:RESult:MM:TDSCdma?" |
|
Function |
Resets the authentication sequence number (SQN) to zero. |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SECurity:AUTHenticate:SQN:RESet" |
|
Function |
Sets/queries the security operations setting:
|
|
Setting |
Range: NONE|AUTHONLY|AUTHINT |
|
Query |
Range: NONE|AUTHONLY|AUTHINT |
|
*RST Setting |
AUTHINT |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SECurity:OPERation AUTHINT" |