For more information on the GPIB Command conventions, see GPIB Command conventions
Function |
Sets/queries the AMR Radio Access Bearer. |
Setting |
Range: AMR475 | AMR515 | AMR590 | AMR670 | AMR740 | AMR795 | AMR1020 | AMR1220 |
Query |
Same as setting |
*RST Setting |
AMR1220 |
Requirements |
Test Application Revision: A.03.00 and above |
Programming Example |
"CALL:SERVice:AMR:RAB AMR1220" |
Function |
Sets/queries the AMR Source. This parameter can only be set when Call/Data Status is Idle. |
Setting |
Range: ECHO | RTVocoder |
Query |
Same as setting |
*RST Setting |
ECHO |
Requirements |
Test Application Revision: A.09.00 and above |
Programming Example |
"CALL:SERVice:AMR:SOURce ECHO" |
Function |
Sets/queries the Speech Echo Loopback Delay. This parameter determines the amount of time that speech frames received on the uplink are delayed before being retransmitted on the downlink. This setting cannot be changed when the cell operating mode is Active Cell and the call/data status is any state other than IDLE, or the test set will reject the change and an error will be reported. |
Setting |
Range: 0.1 to 4 s Resolution: 0.02 |
Query |
Same as setting |
*RST Setting |
0.5 |
Requirements |
Test Application Revision: A.03.00 and above |
Programming Example |
"CALL:SERVice:AMR:SPEech:ECHO:LOOPback:DELay 0.5" |
Function |
Sets/queries the RAB (Radio Access Bearer) configuration used for the GPRS PS Data service. See GPRS Radio Access Bearer. This setting can only be changed while the Call/Data Status is Idle. |
Setting |
Range: GPRS384 |PSDHsdpa64 |PHSPa |
Query |
Same as setting |
*RST Setting |
PSDHsdpa64 (64K UL/HSDPA DL) |
Requirements |
Test Application Revision: A.07.00 and above Test Application Revision: A.08.00 and above, added PHSPa |
Programming Example |
"CALL:SERVice:GPRS:RAB GPRS384" |
Function |
Sets/queries the Channel Type setting. |
Setting |
Range: SRMC12 | MRMC12 | HSDP12 | RMC64 | RMCAM64144 | RMCAM64384 |HSParmc12|R144 |
Query |
same as setting |
*RST Setting |
SRMC12 |
Requirements |
Test
Application Revision: A.03.00 and above Test Application Revision: A.05.00 and above, added HSParmc12 Test Application Revision: A.10.00 and above, added R144 |
Programming Example |
"CALL:SERVice:RBTest:RAB SRMC12" |
Function |
Sets/queries the RB Test Mode RRC State setting. |
Setting |
Range: FACH | DCH |
Query |
same as setting |
*RST Setting |
DCH |
Requirements |
Test Application Revision: A.05.00 and above |
Programming Example |
"CALL:SERVice:RBTest:RRC:STATe DCH" |
Function |
Sets/queries Automatic RRC State Transition Control State. This setting controls whether the automatic RRC state transitions are enabled or not (including the transition based on downlink IP data). This setting cannot be changed while a PDP Context is Active. |
Setting |
Range: 1|ON|0|OFF |
Query |
same as setting |
*RST Setting |
0 (off) |
Requirements |
Test Application Revision: A.10.00 and above |
Programming Example |
"CALL:SERVice:PSData:RRC:TRANsition:AUTO 0" |
Function |
Sets/queries the transaction that are triggered from PDP_ACTIVE state to IDLE. This setting cannot be changed while a PDP Context is Active. |
Setting |
Range: 0.1 to 1800 Increment: 0.1 Unit: s |
Query |
same as setting |
*RST Setting |
5s |
Requirements |
Test Application Revision: A.10.00 and above |
Programming Example |
"CALL:SERVice:PSData:RRC:TRANsition:ITIMer:DCH:VALue 5" |