Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the relative time offset (in 10ms frame) to calculate the activation time parameter included in physical channel reconfiguration message. The activation time parameter is get by: Activation Time = (current CFN + this setting) % 256 |
|
Setting |
Range: 0 to 255 |
|
Query |
Range: 0 to 255 |
|
*RST Setting |
0 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SETup:ACTivation:TIME 255" |
|
Function |
Sets/queries the physical channel reconfiguration target cell UARFCN for TD-SCDMA application. |
|
Setting |
Range: 10054 to 10121, 9404 to 9596, 11504 to 11996, 12484 to 13446 |
|
Query |
Range: 10054 to 10121, 9404 to 9596, 11504 to 11996, 12484 to 13446 |
|
*RST Setting |
10054 |
|
Requirements |
Test Application Revision: A.02.00 and above Test Application Revision: A.0 and above, 11504 to 11996, 12484 to 13446 |
|
Programming Example |
"CALL:SETup:CHANnel:TDSCdma 10054" |
|
Function |
Sets/queries the physical channel reconfiguration uplink closed loop power control step size. |
|
Setting |
Range: 1|2|3 |
|
Query |
Range: 1|2|3 |
|
*RST Setting |
1 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SETup:CLPControl:UPLink:STEPsize 1" |
|
Function |
Sets/queries the physical channel reconfiguration DPCH Type setting. |
|
Setting |
Range: SRMC12|MRMC12 |
|
Query |
Same as setting |
|
*RST Setting |
SRMC12 |
|
Requirements |
Test Application Revision: A.03.00 and above |
|
Programming Example |
"CALL:SETup:DPCHannel:TYPE SRMC12" |
|
Function |
Sets/queries the physical channel reconfiguration DPCH Type State setting. |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 |
|
Requirements |
Test Application Revision: A.03.00 and above |
|
Programming Example |
"CALL:SETup:DPCHannel:TYPE:STATe On" |
|
Function |
Sets/queries physical channel reconfiguration loopback message state. If the state is "ON", the test set sends an open UE test loop message before the physical channel reconfiguration message, and sends a close UE test loop message after receiving the physical channel reconfiguration complete message; else if the state is "OFF", the test set does not send any loop control message. |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0(OFF) |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SETup:LOOPback:MESSage:STATe 0" |
|
Function |
Sets/queries the scrambling code ID of the target cell the UE will be handover to after physical channel reconfiguration. |
|
Setting |
Range: 0 to 127 |
|
Query |
same as setting |
|
*RST Setting |
0 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:SETup:SCODe:IDENtity 0" |
|
Function |
Sets/queries the RB Test Mode to GSM Handover Alerting State. |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (OFF) |
|
Requirements |
Test Application Revision: A.03.00 and above |
|
Programming Example |
"CALL:SETup:SYSTem:GSM:ALERting Off" |