Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the TMSI assignment to be ON/OFF. When the setting is ON, TMSI will be assigned to mobile subscriber after a successful location update procedure, and the test set can page the UE using the TMSI. This parameter can be set in active cell operating mode only when the call status is Idle, or in other operating modes. |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (OFF) |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:TMSI:ASSignment ON" |
|
Function |
Sets/queries the Temporary Mobile Subscriber Identity (TMSI), which shall be used to page if CS Paging Identity Type is set to TMSI. This parameter can be set in active cell operating mode only when the call status is Idle, or in other operating modes. |
|
Setting |
Range: 0 to 4 294 967 294 |
|
Query |
Range: 0 to 4 294 967 294 |
|
*RST Setting |
0 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:TMSI 1348339801" |