Last updated: 2014-11-28
|
Function |
Sets/queries the RF Generator mode:
|
|
Setting |
Range: NORMal | FMBRoadcast |GPS |
|
Query |
Range: NORM | FMBR |GPS |
|
*RST Setting |
NORMal |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGENERATOR:CONFigure NORMal" |
|
Function |
Sets/queries the loss of the FM Adapter. This parameter compensates the loss by increasing the signal strength at the RF OUT ONLY port. |
|
Setting |
Range: -30 to -10 dB Resolution: 0.01 dB |
|
Query |
Same as setting |
|
*RST Setting |
-19.75 dB |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGENERATOR:FMBRoadcast:ADAPter:GAIN -19.75" |
|
Function |
Sets/queries the FM Broadcast mode Amplitude Offset setting that is applied to the RF OUT ONLY port. |
|
Setting |
Range: -50 to 50 dB Resolution: 0.01 dB |
|
Query |
Same as setting |
|
*RST Setting |
0 dB |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGENERATOR:FMBRoadcast:CORRection:GAIN 0" |
|
Function |
Sets/queries whether the FM Broadcast mode Amplitude Offset setting is applied. |
|
Setting |
Range: 1 | ON | 0 | OFF |
|
Query |
Range: 1 | 0 |
|
*RST Setting |
0 | OFF |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGENERATOR:FMBRoadcast:CORRection:STATe 0" |
|
Function |
Sets/queries the frequency at which the test set broadcasts the FM signal. The units (Hz|kHz|MHz|GHz) are optional, if no units are specified then units default to Hz. |
|
Setting |
Range: 10MHz to 110 MHz Resolution: 1 Hz |
|
Query |
Same as setting |
|
*RST Setting |
98.1 MHz |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGENERATOR:FMBRoadcast:FREQuency 100 MHz" |
|
Function |
Sets/queries FM Deviation of the internal audio source. The internal audio source is the amount the modulated signal deviates from the carrier frequency. Operating mode = Test Mode and Downlink Function = CW. The units (Hz|kHz|MHz|GHz) are optional, if no units are specified then units default to Hz. |
|
Setting |
Range: 0 to 75 kHz Resolution: 100 Hz |
|
Query |
Range: 0 to 75 kHz Resolution: 100 Hz |
|
*RST Setting |
22.5 kHz |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGENERATOR:FMBRoadcast:FM:INTernal 22.5 kHz" |
|
Function |
Sets/queries the test set's internal FM frequency. Operating mode = Test Mode and Downlink Function = CW. The units (Hz|kHz|MHz|GHz) are optional, if no units are specified then units default to Hz. |
|
Setting |
Range: 50 to 20,000 Hz Resolution: 1 Hz |
|
Query |
Range: 50 to 20,000 Hz Resolution: 1 Hz |
|
*RST Setting |
1 kHz |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGenerator:FMBRoadcast:FM:INTernal:FREQuency 1 kHz" |
|
Function |
Sets/queries whether the FM Broadcast mode Internal FM Deviation setting is applied. Operating mode = Test Mode and Downlink Function = CW. |
|
Setting |
Range: 1 | ON | 0 | OFF |
|
Query |
Range: 1 | 0 |
|
*RST Setting |
1 (ON) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGENERATOR:FMBRoadcast:FM:INTernal:STATe ON" |
|
Function |
Sets/queries the power at which the test set broadcasts the FM signal. Operating mode = Test Mode and Downlink Function = CW. Note that when this parameters is set to > -30 and < -120, "Over Range" and "Under Range" error message is displayed respectively. |
|
Setting |
Range: -140 to -20 dBm Resolution: 0.01 dBm |
|
Query |
Range: -140 to -20 dBm Resolution: 0.01 dBm |
|
*RST Setting |
-50 dBm |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGENERATOR:FMBRoadcast:POWer -50 dBm" |
|
Function |
Sets/queries whether the FM Broadcast Power setting is applied. |
|
Setting |
Range: 1 | ON | 0 | OFF |
|
Query |
Range: 1 | 0 |
|
*RST Setting |
1 (OFF) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGENERATOR:FMBRoadcast:POWer:STATe ON" |
|
Function |
Sets/queries the RF Gen Freq. If no units are specified the setting defaults to Hz. |
|
Setting |
Range: 292 MHz to 2700 MHz Resolution: 0.1 Hz |
|
Query |
Same as setting |
|
*RST Setting |
851 MHz |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGenerator:FREQuency 2015 MHZ" |
|
Function |
Sets/queries the filter that is used to filter the GPS baseband signal when the operating mode is CW and the RF Gen Config is GPS . A Gaussian or Rectangle filter with 10 MHz bandwidth is supported in this setting.. |
|
Setting |
Range: GAUSsian | RECTangle |
|
Query |
Range: GAUS | RECT |
|
*RST Setting |
GAUSsian |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGenerator:GPS:BFILter GAUS" |
|
Function |
Queries the frequency of RF source 1 when the operating mode is CW and the RF Gen Config is GPS. This parameter is fixed at 1575.42MHz and can be queried only. |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGenerator:GPS:FREQuency?" |
|
Function |
Queries the frequency of RF source 2 when the operating mode is CW and the RF Gen Config is GPS. |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGenerator:GPS:FREQuency2?" |
|
Function |
Sets/queries the type of GPS navigation message that is transmitted on GPS frames.
|
|
Setting |
Range: DEFault | RAW |
|
Query |
Range: DEF| RAW |
|
*RST Setting |
DEFault |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGenerator:GPS:NMESsage DEF" |
|
Function |
Sets/queries the power at which the test set generates the GPS signal. Setting this parameter is also set the GPS State to ON. |
|
Setting |
Range: -160dBm to -20dBm, after the Amplitude Offset (optional) has been included. Resolution: 0.01 dBm |
|
Query |
same as setting |
|
*RST Setting |
-80 dBm |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGenerator:GPS:POWer -80" |
|
Function |
Sets/queries the power at which the test set generates the GPS signal. |
|
Setting |
Range: -160dBm to -20dBm, after the Amplitude Offset (optional) has been included. Resolution: 0.01 dBm |
|
Query |
same as setting |
|
*RST Setting |
-80dBm |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGenerator:GPS:POWer:AMPLitude -80" |
|
Function |
Sets/queries whether the GPS power setting is applied. |
|
Setting |
Range: 1 | ON | 0 | OFF |
|
Query |
Range: 1 | 0 |
|
*RST Setting |
1 | ON |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGenerator:GPS:POWer:STATe ON" |
|
Function |
Sets/queries the date type that is transmitted on GPS frames. |
|
Setting |
Range: PN9| PN15 |
|
Query |
same as setting: |
|
*RST Setting |
PN9 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGenerator:GPS:RAW:PPATtern PN9" |
|
Function |
Sets/queries which satellite is generating the GPS signal. |
|
Setting |
Range: 1 to 37 Resolution: 1 |
|
Query |
same as setting: |
|
*RST Setting |
1 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:RFGenerator:GPS:SVID 1" |