Home > Configuration > Control > Format Switch
Last updated: 2014-11-28
Some radio formats are combined as fast switching applications. For example, the E1969A TD-SCDMA_GSM fast switch test application allows you to switch between GSM/GPRS/EGPRS and TD-SCDMA formats very quickly (in less than 2 seconds) if the required license is available.
To fast switch between TD-SCDMA and GSM/GPRS/EGPRS test applications, refer to Fast Switch Between TD-SCDMA and GSM.
GPIB Commands: SYSTem:APPLication:FORMat[:NAME]