Last updated: 2014-11-28
The INITiate subsystem is used to:
Start (activate) individual or multiple (concurrent) measurements.
Turn individual measurements off.
Determine the number of measurements currently active (INIT:COUNT?).
Determine the names of the measurements currently active (INIT:ON?).
Determine which measurements are finished (INIT:DONE?).
When a measurement is started using INITiate commands, a new measurement cycle is started. If the selected measurement is currently in a measurement cycle, it is aborted. If a timeout is specified, the timeout period begins when a measurement is initiated.