Last updated: 2014-11-28
When Power Control is set to Auto, the test set sets its receiver input power level to the value of the MS DPCH Tgt Pwr setting (see Expected Power ).
The maximum setting allowed for MS DPCH Tgt Pwr is +30 dBm.
GPIB Commands: CALL:MS:POWer:TARGet[:AMPLitude]