Last updated: 2014-11-28
RF IN/OUT
This Type-N connector is the default path for all RF signals out of the test set, and is always used as the RF input. Refer to the Technical Specifications in the Application Datasheet for more information.
RF OUT ONLY
This Type-N connector is an optional path for all RF signals out of the test set. It is intended to be used for duplexed testing. Front panel selection of this port is provided by the RF Output Port ( F6 ) control on the System Config screen, and by the RFGenerator:OUTPut[:DESTination] IO/OUT command. The same amplitude offsets and output power settings are used for either selected port (RF IN/OUT or RF OUT ONLY). Refer to the Technical Specifications in the Application Datasheet for more information.
GPIB Commands: RFGenerator