Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Turns on/off the auto Measurement Frequency which determines the measurement downconverter signal path frequency control mode. ON = automatic OFF = manual (see RFANalyzer:MANual:MEASurement[:MFRequency]) |
|
Setting |
Range:0 | OFF | 1 | ON |
|
Query |
Range:0 | 1 |
|
*RST Setting |
1 | ON |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"RFANalyzer:CONTrol:MEASurement:FREQuency:AUTO OFF" |
|
Function |
Sets/queries power control . ON = automatic OFF = manual |
|
Setting |
Range:0 | OFF | 1 | ON |
|
Query |
Range:0 | 1 |
|
*RST Setting |
1 |ON |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"RFANalyzer:CONTrol:POWer:AUTO OFF" |
|
Function |
Sets/queries the expected CW receiver input power. This setting is only used when the operating mode is set to CW. |
|
Setting |
Range: -29 dBm to +44 dBm |
|
Query |
same as setting |
|
*RST Setting |
+13 dBm |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"RFANALYZER:CW:EXPECTED:POWER -20" |
|
Function |
The setting form of this command performs two functions: (1) sets Measurement Frequency , the tune frequency of the test set's measurement signal path, and (2) selects manual tune mode for the test set's measurement signal path. The query form of this command returns the tune frequency of the test set's measurement signal path. |
|
Setting |
Range: 292.5 MHz to 2700 MHz Resolution: 0.1 Hz |
|
Query |
same as setting |
|
*RST Setting |
896.000 MHz |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"RFANALYZER:MANUAL:MEASUREMENT:MFREQUENCY 896 MHZ" |
|
Function |
Sets/queries the frequency of measurement frequency when the frequency mode is manual. |
|
Setting |
Range: 292.5 MHz to 2700 MHz Resolution: 0.1 Hz |
|
Query |
same as setting |
|
*RST Setting |
896.000 MHz |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"RFANALYZER:MANUAL:MEASUREMENT:FREQUENCY 896 MHZ" |
|
Function |
Sets/queries manual power. |
|
Setting |
Range: Test application and system type dependent (approximately-69 to + 31 dBm). Resolution: 0.01 dBm |
|
Query |
same as setting |
|
*RST Setting |
0 dBm |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"RFANALYZER:MANUAL:POWER:SELECTED 24 DBM" |
|
Function |
Sets/queries manual power when TDSCdma is the current system type. |
|
Setting |
Range: -70 dBm to +30 dBm actual hardware range with amplitude offset = 0 Resolution: 0.01 dBm |
|
Query |
same as setting |
|
*RST Setting |
0 dBm |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"RFANalyzer:MANual:POWer:TDSCdma 24 DBM" |
|
Function |
Turns on/off the auto Uplink Frequency which determines the test set's demodulation signal path frequency control mode. ON = automatic OFF = manual |
|
Setting |
Range:0 | OFF | 1 | ON |
|
Query |
Range:0 | 1 |
|
*RST Setting |
1 | ON |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"RFANalyzer:CONTrol:UPLink:FREQuency:AUTO OFF" |
|
Function |
The setting form of this command performs two functions: (1) sets uplink Frequency , the tune frequency of the test set's demodulation signal path, and (2) selects manual tune mode for the test set's demodulation signal path. The query form of this command returns the tune frequency of the test set's demodulation signal path. |
|
Setting |
Range: 292.5 MHz to 2700 MHz Resolution: 0.1 Hz |
|
Query |
same as setting |
|
*RST Setting |
896 MHz |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"RFANALYZER:MANUAL:UPLINK:MFREQUENCY 896 MHZ" |
|
Function |
Sets/queries the frequency of uplink frequency when the frequency mode is manual. |
|
Setting |
Range: 292.5 MHz to 2700 MHz Resolution: 0.1 Hz |
|
Query |
same as setting |
|
*RST Setting |
896 MHz |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"RFANALYZER:MANUAL:UPLINK:FREQUENCY 896 MHZ" |