Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
For the measurement, see Loopback Bit Error Ratio (BER) Measurement.
|
Function |
Sets/queries the Bad CRC Block which determines whether the data block is counted for BER calculation. See Bad CRC Block. |
|
Setting |
Range: EXCLude | INCLude |
|
Query |
Range: EXCL | INCL |
|
*RST Setting |
EXCLude |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TBERror:BCRC EXCLude" |
|
Function |
Sets/queries Confidence State. See Confidence State. |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (Off) |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TBERror:CONFidence:STATe OFF" |
|
Function |
Sets/queries the trigger arm state for the loopback BER measurement. The trigger arm state determines whether the loopback BER measurement will be made once then stop (0|OFF (single)), or automatically re-arm upon completion of one measurement and repeat the process (1|ON (continuous)). |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (OFF) |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETUP:TBERror:CONTinuous OFF" |
|
Function |
Sets/queries the number of bits to test. See Number of bits to test. |
|
Setting |
Range: 1000 to 999 999 999 Resolution: 1 |
|
Query |
same as setting |
|
*RST Setting |
10000 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TBERror:COUNt 10000" |
|
Function |
Sets/queries the BER Requirement, in percent. When the confidence state is On, as testing progresses the bit error ratio trajectory converges to a BER value, which shall not be exceed this setting as test requirement. See BER Requirement. |
|
Setting |
Range: 0.10 to 50.00 Resolution: 0.01 |
|
Query |
Range: 0.10 to 50.00 |
|
*RST Setting |
0.10 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TBERror:RATio:REQuirement 0.1" |
|
Function |
The setting form of this command performs two functions: (1) sets the loopback BER measurement's timeout value, and (2) sets the loopback BER measurement's timeout state to 1 (ON). The query form returns the loopback BER measurement's timeout value. |
|
Setting |
Range: 0.1 to 999.9 seconds Unit: S | MS | US | NS |
|
Query |
Range: 0.1 to 999.9 |
|
*RST Setting |
10 s, on |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TBERror:TIMeout:STIMe 5S" |
|
Function |
Sets/queries the loopback BER measurement's timeout state. |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0(OFF) |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TBERror:TIMeout:STATe ON" |
|
Function |
Sets/queries the loopback BER measurement's timeout. |
|
Setting |
Range: 0.1 to 999.9 seconds Unit: S | MS | US | NS |
|
Query |
Range: 0.1 to 999.9 |
|
*RST Setting |
10 s |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TBERror:TIMeout:TIME 5S" |