Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions.
For the closed loop power control measurement description, see Closed Loop Power Control (CLPC) Measurement.
|
Function |
Sets/queries the lower limit and the upper limit of the maximum absolute power among all measured steps, in a comma-separated manner. |
|
Setting |
Range: -80 to 40 dBm (lower limit), -80 to 40 dBm (upper limit) Resolution:0.01 |
|
Query |
same as setting |
|
*RST Setting |
21,25 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TCLPower:MAXimum:POWer:LIMit 21,25" |
|
Function |
Sets/queries the upper limit of the minimum absolute power among all measured steps. |
|
Setting |
Range:-80 to 40 dBm Resolution:0.01 |
|
Query |
same as setting |
|
*RST Setting |
-49 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TCLPower:MINimum:POWer:LIMit -49" |
|
Function |
Sets/queries the number of DOWN and UP TPC commands sent to the UE, in a comma-separated manner. |
|
Setting |
Range: 0 to 150 (the number of DOWN TPC commands), 0 to 150 (the number of UP TPC commands) Resolution: 1 |
|
Query |
same as setting |
|
*RST Setting |
100,100 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TCLPower:NStep 50,50" |
|
Function |
Sets/queries the check offset to the maximum and the minimum power, in a comma-separated manner. The maximum/minimum power is the maximum/minimum power among all measured steps. |
|
Setting |
Parameters are two check offsets separated by comma, representing offset to the maximum power comes first and offset to the minimum power comes second, respectively. For each offset:
|
|
Query |
same as setting |
|
*RST Setting |
0.5, 0.5 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TCLPower:OFFSet 0.5,0.5" |
|
Function |
Sets/queries the lower and upper limit (in a comma-separated manner) for either REL1POW or REL10POW when in TD-SCDMA Test operating mode.
|
|
Setting |
Range:
Resolution:0.01 |
|
Query |
same as setting |
|
*RST Setting |
|
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TCLPower:STEP10:LIMIT 10.0,30.0" |
|
Function |
Sets/queries the lower and upper limit (in a comma-separated manner) for either REL1POW or REL10POW when the step size is set to 1dB in Active Cell operating mode.
|
|
Setting |
Range:
Resolution:0.01 |
|
Query |
same as setting |
|
*RST Setting |
|
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TCLPower:STEP10:LIMit:DB1 10.0,30.0" |
|
Function |
Sets/queries the lower and upper limit (in a comma-separated manner) for either REL1POW or REL10POW when the step size is set to 2dB in Active Cell operating mode.
|
|
Setting |
Range:
Resolution:0.01 |
|
Query |
same as setting |
|
*RST Setting |
|
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TCLPower:STEP10:LIMit:DB2 10.0,30.0" |
|
Function |
Sets/queries the lower and upper limit (in a comma-separated manner) for either of the two cases (REL1POW or REL10POW) when the step size is set to 3dB in Active Cell operating mode, so that
|
|
Setting |
Range:
Resolution:0.01 |
|
Query |
same as setting |
|
*RST Setting |
|
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TCLPower:STEP10:LIMit:DB3 10.0,30.0" |
|
Function |
The setting form of this command performs two functions: (1) sets the closed loop power control measurement's timeout value, and (2) sets the measurement's timeout STATe to 1 (on) |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second Unit: S | MS | US | NS (If no units are specified in the command then 'S' is used as the default) |
|
Query |
Range: 0.1 to 999.9 seconds |
|
*RST Setting |
10 seconds,off |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TCLPower:TIMeout:STIMe 5 S" |
|
Function |
Sets/queries the closed loop power control measurement's timeout (see Measurement Timeouts ) state |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETUP:TCLPOWER:TIMEOUT:STATE ON" |
|
Function |
Sets/queries the closed loop power control measurement's timeout setting to be used when the timeout state is set to ON. |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second Unit: S | MS | US | NS (If no units are specified in the command then 'S' is used as the default) |
|
Query |
Range: 0.1 to 999.9 seconds |
|
*RST Setting |
10 seconds |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TCLPower:TIMeout:TIMe 5 S" |
|
Function |
Sets/queries the Trigger Delay setting of the closed loop power control measurement. |
|
Setting |
Range: -10 to 10 ms Resolution: 0.1 us |
|
Query |
Range: -10 to 10 ms Resolution: 0.1 us |
|
*RST Setting |
0ms |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TCLPower:TRIGger:DELay 1 MS" |
|
Function |
Sets/queries the Trigger Source of the closed loop power control measurement. |
|
Setting |
Range: RISE | EXTernal | PROTocol |
|
Query |
Range: RISE | EXT | PROT |
|
*RST Setting |
PROT |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TCLPower:TRIGger:SOURce PROTocol" |