Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions.
For the channel power measurement, see Channel Power Measurement.
|
Function |
Sets/queries the trigger arm state for the channel power measurement. The trigger arm state determines whether the channel power measurement will be made once then stop (0|OFF (single)), or automatically re-arm upon completion of one measurement and repeat the process (1|ON (continuous)). |
|
Setting |
Range:1|ON|0|OFF |
|
Query |
Range:1|0 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETUP:TCPOWER:CONTINUOUS OFF" |
|
Function |
The setting form of this command performs two functions: (1) sets the number of channel power measurements to be made in a multi-measurement, and (2) sets the multi-measurement STATe command to 1 (on). The query form returns the number of channel power multi-measurements to be made when multi-measurement state is ON. |
|
Setting |
Range:1 to 999 |
|
Query |
Range:1 to 999 |
|
*RST Setting |
Off (10 when STATe = On) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETUP:TCPOWER:COUNT:SNUMBER 5" |
|
Function |
Sets/queries the number of channel power measurements to be made when the multi-measurement state is ON. |
|
Setting |
Range:1 to 999 |
|
Query |
Range:1 to 999 |
|
*RST Setting |
10 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETUP:TCPOWER:COUNT:NUMBER 5" |
|
Function |
Sets/queries the channel power multi-measurement state. |
|
Setting |
Range:1|ON|0|OFF |
|
Query |
Range:1|0 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETUP:TCPOWER:COUNT:STATE ON" |
|
Function |
Sets/queries the state of the root-raised cosine (RRC) filter. |
|
Setting |
Range:1|ON|0|OFF |
|
Query |
Range:1|0 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETUP:TCPOWER:FILTER:RRC ON" |
|
Function |
Sets/queries the value of Manual Power Range Offset. |
|
Setting |
Range:-25dB to 25dB Resolution: 0.01 dB Unit: dB |
|
Query |
Range:-25dB to 25dB |
|
*RST Setting |
0.00dB |
|
Requirements |
Test Application Revision: A.06.00 and above |
|
Programming Example |
"SETup:TCPOWER:POWer:RANGe:OFFSet:MANual 6dB" |
|
Function |
The setting form of this command performs two functions: (1) sets the channel power measurement's timeout value, and (2) sets the channel power measurement's timeout STATe to 1 (on). The query form returns the channel power measurement's timeout value. |
|
Setting |
Range:0.1 to 999.9 seconds Resolution: 0.1 second Unit: S | MS | US | NS |
|
Query |
Range:0.1 to 999.9 |
|
*RST Setting |
10 seconds, on |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETUP:TCPOWER:TIMEOUT:STIME 5 S" |
|
Function |
Sets/queries the channel power measurement's timeout state. |
|
Setting |
Range:1|ON|0|OFF |
|
Query |
Range:1|0 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETUP:TCPOWER:TIMEOUT:STATE ON" |
|
Function |
Sets/queries the channel power measurement's timeout setting to be used when the timeout state is set to ON. |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second Unit: S | MS | US | NS |
|
Query |
Range: 0.1 to 999.9 |
|
*RST Setting |
10 seconds |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETUP:TCPOWER:TIMEOUT:TIME 5 S" |
|
Function |
Sets/queries the channel power measurement's Trigger Source . |
|
Setting |
Range: AUTO | IMMediate | RISE |EXTernal | PROTocol |
|
Query |
AUTO | IMM | RISE |EXT| PROT |
|
*RST Setting |
AUTO |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETUP:TCPOWER:TRIGGER:SOURCE IMMEDIATE" |
|
Function |
Sets/queries the channel power measurement's Trigger Delay setting. |
|
Setting |
Range:-10 to 10 ms Resolution: 0.1 usec Unit: S | MS | US | NS |
|
Query |
Same as setting |
|
*RST Setting |
0 seconds |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETUP:TCPOWER:TRIGGER:DELAY 1MS" |
|
Function |
Sets/queries which uplink time slot to be measured. |
|
Setting |
Range: TS1 | TS2 | TS3 |TS4 |
|
Query |
Same as setting |
|
*RST Setting |
TS1 |
|
Requirements |
Test Application Revision: A.06.00 and above |
|
Programming Example |
"SETup:TCPOWER:TSLot:MEASure TS1" |