Show 

Home > Measurements > Channel Power Measurement

Channel Power Measurement

Last updated: 2010-03-31

Channel Power Measurement Description

Channel Power Measurement Parameters

Channel Power Measurement Results

Input Signal Requirements

Channel Power Measurement Description

The channel power measurement is made on the RF input signal after frequency downconversion and an analog to digital conversion. The actual power measurement is performed by the test set's digital signal processor (DSP).

The channel power measurement is used to measure the following power as defined in TS 34.122 Section 3.1.

This measurement requires the calibration data of the measurement receiver path gain, which are part of the results of the measurement calibration, see Calibrate Measurements.

Channel Power Measurement Parameters

Channel Power Measurement Results

Input Signal Requirements

Related Topics

GPIB Commands: SETup:TCPower, FETCh:TCPower