Last updated: 2010-06-12
For more information on the GPIB Command conventions, see GPIB Command conventions
For the measurement, see Open Loop Power Control (OLPC) Measurement
|
Function |
Sets/queries the Initial UpPCH Tx Power Limit for the open loop power control measurement. The result fails if the difference between the measured power and the expected power is larger than this limit. |
|
Setting |
Range: 0 to 20 dB Resolution: 0.01 |
|
Query |
Same as setting |
|
*RST Setting |
9 |
|
Requirements |
Test Application Revision: A.03.00 and above |
|
Programming Example |
"SETup:TOLPower:LIMit 9" |
|
Function |
The setting form of this command performs two functions: (1) sets the open loop power control measurement's timeout value, and (2) sets the open loop power control measurement's timeout state to 1 (on). The query form returns the open loop power control measurement's timeout value. |
|
Setting |
Range: 0.1 to 999.9 seconds Unit: S | MS | US | NS |
|
Query |
Same as setting |
|
*RST Setting |
10 s, on |
|
Requirements |
Test Application Revision: A.03.00 and above |
|
Programming Example |
"SETup:TOLPower:TIMeout 10s" |
|
Function |
Sets/Queries the open loop power control measurement's timeout state. |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0(OFF) |
|
Requirements |
Test Application Revision: A.03.00 and above |
|
Programming Example |
"SETup:TOLPower:TIMeout:STATe ON" |
|
Function |
Sets/queries the open loop power control measurement's timeout. |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second Unit: S | MS | US | NS |
|
Query |
Range: 0.1 to 999.9 |
|
*RST Setting |
10 s |
|
Requirements |
Test Application Revision: A.03.00 and above |
|
Programming Example |
"SETup:TOLPower:TIMeout:TIME 5S" |