Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions.
For the measurement, see Spectrum Emission Mask (SEM) Measurement.
|
Function |
Sets/queries the trigger arm state for the Spectrum Emission Mask measurement. The trigger arm state determines whether the measurement will be made once then stop (0|OFF (single)) or automatically re-arm upon completion of one measurement and repeat the process (1|ON (continuous)). |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0(Off) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETUP:TSEMASK:CONTINUOUS OFF" |
|
Function |
Sets/queries the number of the Spectrum Emission Mask measurement to be made in a multi-measurement setup. This command sets the count, and automatically sets the multi-measurement STATe command to 1 (on). |
|
Setting |
Range: 1 to 999 |
|
Query |
Range: 1 to 999 |
|
*RST Setting |
Off (10 when STATe = On) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TSEMask:COUNt:SNUMber 5" |
|
Function |
Sets/queries the number of the Spectrum Emission Mask measurement to be made when multi-measurement state is ON: |
|
Setting |
Range: 1 to 999 |
|
Query |
Range: 1 to 999 |
|
*RST Setting |
10 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TSEMask:COUNt:NUMber 5" |
|
Function |
Sets/queries the multi-measurement state of Spectrum Emission Mask measurement. |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range:1|0 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETUP:TSEMask:COUNT:STATE ON" |
|
Function |
Sets/queries the pass/fail limits for the following frequency offsets in the Spectrum Emission Mask measurement:
|
|
Setting |
Range:-80 to 10 dBc |
|
Query |
Range:-80 to 10 dBc |
|
*RST Setting |
|
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TSEMask:LIMit -35,-49,-59,-44,-44" |
|
Function |
Sets/queries the value of Manual Power Range Offset. |
|
Setting |
Range:-25dB to 25dB Resolution: 0.01 dB Unit: dB |
|
Query |
Range:-25dB to 25dB |
|
*RST Setting |
0.00dB |
|
Requirements |
Test Application Revision: A.06.00 and above |
|
Programming Example |
"SETup:TSEMask:POWer:RANGe:OFFSet:MANual 6dB" |
|
Function |
(1) sets the Spectrum Emission Mask measurement's timeout value, (2) sets the measurement's timeout STATe to 1 (on) |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second |
|
Query |
Range: 0.1 to 999.9 seconds |
|
*RST Setting |
10 seconds,off |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TSEMask:TIMeout:STIMe 5 S" |
|
Function |
Sets/queries the Spectrum Emission Mask measurement's timeout setting to be used when the timeout state is set to ON. |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second |
|
Query |
Range: 0.1 to 999.9 seconds |
|
*RST Setting |
10 seconds |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TSEMask:TIMeout:TIMe 5 S" |
|
Function |
Sets/queries the Trigger Source of the Spectrum Emission Mask measurement. |
|
Setting |
Range:AUTO | IMMediate | RISE | EXTernal | PROTocol |
|
Query |
Range:AUTO | IMM | RISE | EXT | PROT |
|
*RST Setting |
AUTO |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TSEMask:TRIGger:SOURce IMMEDIATE" |
|
Function |
Sets/queries the Trigger Delay setting of the Spectrum Emission Mask measurement: This setting can be used to delay the measurement trigger in order to start a measurement during a specific timeslot in the frame. |
|
Setting |
Range: -10 to 10 ms Resolution: 0.1 us |
|
Query |
Range: -10 to 10 ms Resolution: 0.1 us |
|
*RST Setting |
0ms |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TSEMask:TRIGger:DELay 1MS" |
|
Function |
Sets/queries which uplink time slot to be measured. |
|
Setting |
Range: TS1 | TS2 | TS3 |TS4 |
|
Query |
Same as setting |
|
*RST Setting |
TS1 |
|
Requirements |
Test Application Revision: A.06.00 and above |
|
Programming Example |
"SETup:TSEMask:TSLot:MEASure TS1" |