SYSTem:CONFigure

Last updated: 2014-11-28

For more information on the GPIB Command conventions, see GPIB Command conventions

SYSTem:CONFigure:INFormation:HARDware:VERBose?

Function

Query the manufacturer, model number, model number of the test application running, serial number, revision, board ID, and cal file information. The information provided by the query represents the configuration that existed when the test set was powered up.

*RST Setting

Resets have no effect on this information. The information is gathered during the power up cycle.

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SYSTEM:CONFIGURE:INFORMATION:HARDWARE:VERBOSE?"