Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
Function |
Query the model number of the test application running. Printable ASCII characters up to a 15 character string. |
Query |
Range: ASCII codes 32 - 126 decimal excluding comma and semicolon |
*RST Setting |
non volatile, read from the test set's hard disk |
Requirements |
Test Application Revision: A.01.00 and above |
Programming Example |
"SYSTem:CURRent:TA:MODel?" |
Function |
Query the name of the test application running. Printable ASCII characters up to a 25 character string. This command is not recommended. |
Query |
Range: ASCII codes 32 - 126 decimal excluding comma and semicolon. |
*RST Setting |
non volatile, read from the test set's hard disk |
Requirements |
Test Application Revision: A.01.00 and above |
Programming Example |
"SYSTem:CURRent:TA:NAME?" |
Function |
Query the coordinated codeware revision for the test application running. Printable ASCII characters up to a 20 character string. This command is not recommended. |
Query |
Range: ASCII codes 32 - 126 decimal excluding comma and semicolon |
*RST Setting |
non volatile, read from the test set's hard disk. |
Requirements |
Test Application Revision: A.01.00 and above |
Programming Example |
"SYSTem:CURRent:TA:REVision?" |