Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
Function |
Queries the contents of the Error/Event Queue. The Error/Event Queue may contain one or more messages with an error or event description. Manual users may view the Message Log from the SYSTEM CONFIG screen. See Message Log . The contents of the Error/Event Queue and the Message Log may not match. For example, Manual User Error Messages are not returned by the SYSTem:ERRor? query, they are only viewable from the Error Message Log. |
Query |
Error/Event Queue Range: 0 to 100 messages up to 255 characters in length |
Requirements |
Test Application Revision: A.01.00 and above |
Programming Example |
"SYSTem:ERRor?" |