Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
Function |
Queries the current internal operating temperature. |
Query |
Range: -60.0 to 100.0 (°C) |
Requirements |
Test Application Revision: A.01.00 and above |
Programming Example |
"SYSTem:INSTrument:TEMPerature?" |
Function |
Starts the Thermal Power Null Adjustment . Note: you should ensure that your test set has warmed up at least 30 minutes and that no power is present at the front panel RF connectors before performing any calibrations. When this adjustment has completed, a value is returned to indicate the success or failure of the adjustment. 0 indicates the adjustment completed successfully, 1 indicates that it failed. |
Query |
Range: 0 (success), 1 (failure) |
Requirements |
Test Application Revision: A.01.00 and above |
Programming Example |
"SYSTem:INSTrument:THERmal:POWer:NULL:ADJust?" |