Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
GPIB Command to Clear the UI Log |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTem:LOG:UI:CLEAR" |
|
Function |
Query the number of lines containing GPIB commands in the UI Log. |
|
Query |
returns the number of lines in the log since the last time the log was cleared. |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTem:LOG:UI:COUNt?" |
|
Function |
Sets/queries the UI log GPIB state. |
|
Setting |
Range: ON|OFF |
|
Query |
Range: 1(ON)|0(OFF) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTem:LOG:UI:GPIB ON" |
|
Function |
Query the string at the specified line in the UI Log. The GPIB query in the following table returns the string located at the line in the log that you specify. Note that issuing this command turns off GPIB logging. You must turn it back on using the SYSTem:LOG:UI:GPIB[:STATe] command to continue GPIB logging. |
|
Setting |
Range: An integer |
|
Query |
Range: the string located at the line in the log that you specify. |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTem:LOG:UI:REPort?" |