SYSTem:SYNChronized

Last updated: 2014-11-28

For more information on the GPIB Command conventions, see GPIB Command conventions

SYSTem:SYNChronized

Function

Sets/queries the test set to see that all prior sequential commands have completed or that all prior overlapped commands have started, indicating that the input buffer is synchronized.

Setting

Bit 12 of the status operation condition register is pulsed.

Query

Range: 1

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SYSTem:SYNChronized?"