UE Measurement Control

Last updated: 2010-03-10

Description

When there is an active connection between the UE and the test set, the UE can perform measurements on the test set's downlink signal and report the measurement results. By pressing the Send Measurement Request (F1) on the front panel or sending the CALL:MS:REPorted:MEASurement:REQuest command, the test set sends a single measurement control message to the UE, with the following measurement information:

You can view the measurement result either from the front panel, or retrieve it using the GPIB command (See CALL:MS:REPorted[:CELL]:PRIMary:CCPChannel:RSCP?).

Measurement Results

Reported value

Measured quantity value

Unit

P-CCPCH RSCP_LEV _-05

P-CCPCH RSCP <-120

dBm

P-CCPCH RSCP_LEV _-04

-120 <=P-CCPCH RSCP < -119

dBm

P-CCPCH RSCP_LEV _-03

-119 <=P-CCPCH RSCP < -118

dBm

…

…

…

P-CCPCH RSCP_LEV _89

-27 <=P-CCPCH RSCP < -26

dBm

P-CCPCH RSCP_LEV _90

-26 <=P-CCPCH RSCP < -25

dBm

P-CCPCH RSCP_LEV _91

-25 <=P-CCPCH RSCP

dBm

This measurement results can be cleared by sending a new Measurement Request or Partial/Full Preset operation.