Last updated: 2010-03-10
This setting is only available to TD-SCDMA Test Operating mode.
When UL DPCH TFCI Ctrl is set to Manual, this setting determines which TFC the test set expects from the UE on the uplink DPCH.
GPIB Commands: CALL:TDTest:UPLink:TFCIndicator:MANual