Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the Uplink Closed Loop Power Control Mode in TD-SCDMA operating mode. |
|
Setting |
Range:DOWN | UP | ALTernating | ACTive |
|
Query |
Range:DOWN | UP | ALT | ACT |
|
*RST Setting |
ALTernating |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:TDTest:CLPControl:UPLink:MODE UP" |
|
Function |
The setting form of this command performs two functions: (1) sets the TD-SCDMA Test DL DPCH level and (2) sets TD-SCDMA Test DL DPCH level state to on. The query form of this command returns the TD-SCDMA Test DL DPCH level. |
|
Setting |
Range:-30.00 dB to 0 dB Resolution:0.01 |
|
Query |
Same as setting |
|
*RST Setting |
0dB |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:TDTest:DPCHannel -7" |
|
Function |
Sets/queries the TD-SCDMA Test DL DPCH level state. |
|
Setting |
Range:On|Off |
|
Query |
Range:1|0 |
|
*RST Setting |
On |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:TDTest:DPCHannel:STATe ON" |
|
Function |
Sets/queries the TD-SCDMA Test DL DPCH level offset. |
|
Setting |
Range:-30.00 dB to 0 dB Resolution:0.01 |
|
Query |
Same as setting |
|
*RST Setting |
0dB |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:TDTest:DPCHannel:LEVel -7" |
|
Function |
Sets/queries the TD-SCDMA Test DL PICH Data . The pattern can be set to either all ones or all zeros. |
|
Setting |
Range: ZERos | ONES |
|
Query |
Range: ZER | ONES |
|
*RST Setting |
ZERos |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:TDTest:PICHannel:DATA ZER" |
|
Function |
Sets/queries the TD-SCDMA Test DL TFCI Pattern. |
|
Setting |
Range: "00" to "1F" |
|
Query |
Same as setting |
|
*RST Setting |
"00" |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:TDTest:TFCIndicator '00'" |
|
Function |
Sets/queries the TD-SCDMA Test UL DPCH midamble configuration. |
|
Setting |
Range:2, 4, 6, 8, 10, 12, 14, 16 |
|
Query |
Same as setting |
|
*RST Setting |
+8 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:TDTest:UPLink:DPCHannel:MCONfig 8" |
|
Function |
Sets/queries the TD-SCDMA Test UL DPCH midamble shift. |
|
Setting |
Range:1 to 16 |
|
Query |
Same as setting |
|
*RST Setting |
+1 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:TDTest:UPLink:DPCHannel:MSHift 1" |
|
Function |
Sets/queries the TD-SCDMA Test UL TFCI control: If the setting is 1(auto mode), the test set uses the received TFCI from UE; else the setting is 0(manual mode), the test set uses the TFCI set by CALL:TDTest:UPLink:TFCIndicator:MANual command. |
|
Setting |
Range:1|ON|0|OFF |
|
Query |
1|0 |
|
*RST Setting |
0 (manual) |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:TDTest:UPLink:TFCIndicator:CONTrol:AUTO 1" |
|
Function |
Sets/queries manual uplink TFCI that controls which transport format combination the test set expects from the uplink DPCH. This setting is only applicable when CALL:TDTest:UPLink:TFCIndicator:CONTrol:AUTO is set to OFF (manual). |
|
Setting |
Range:NONE|DCCHannel|DTCHannelDTDCchannel |
|
Query |
1 to 4 |
|
*RST Setting |
DCCHannel |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:TDTest:UPLink:TFCIndicator:MANual DCCHannel" |