Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the downlink channel number. This setting cannot be changed while in active cell operating mode and the call status is not IDLE. Attempting to change this setting under those conditions results in the following error message:"TD-SCDMA call operation rejected; Change allowed only when 23 Call Status is Idle." Use other operating modes when changing this setting. After successful completion of a Physical Channel Reconfiguration, the setting will be set the same to the value of physical channel reconfiguration target Cell UARFCN. |
|
Setting |
Range:10054 to 10121, 11504 to 11996, 9404 to 9596, 12484 to 13446 |
|
Query |
Range:10054 to 10121, 11504 to 11996, 9404 to 9596, 12484 to 13446 |
|
*RST Setting |
10087 |
|
Requirements |
Test Application Revision: A.01.00 and above Test Application Revision: A.08.00 and above, added 11504 to 11996, 12484 to 13446 |
|
Programming Example |
"CALL:CHANnel 10087" |