Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the frequency control mode of test set. When the setting is ON, the frequency is specified by a channel number (UARFCN) in auto frequency control mode; when the setting is OFF, the frequency is independently in manual frequency control mode, see CALL:CELL:RFGenerator:FREQuency. |
|
Setting |
Range:1|ON|0|OFF |
|
Query |
Range:1|0 |
|
*RST Setting |
1 (auto) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:CONTrol:DOWNlink:FREQuency:AUTO ON" |